require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
December 9, 2021
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation (“Toshiba”) announces the MN09, a massive capacity 18TB [1] addition to its NAS HDD line-up.
High growth in data creation is driving demand for higher storage capacities, and work-from-home customers need fast access to data and the ability to archive and share data in private cloud environments. The 18TB MN09 delivers greater storage capacity and power efficiency to meet the growing needs of storage customers.
MN09 is a 9-disk helium-sealed conventional magnetic recording (CMR) drive that leverages Toshiba’s new innovative Flux Control Microwave-Assisted Magnetic Recording (FC-MAMR™) technology. FC-MAMR™ advances CMR capacity to 18TB and delivers increased density per platter over previous designs. The MN09 is the 3rd generation to use Toshiba’s pioneering 9-disk helium-sealed mechanical design.
MAMR technology is one solution that extends HDD data capacities. The ability of HDD using a new MAMR head to significantly improve the write ability of the Microwave Assisted Switching (MAS) effect has been developed recently. Toshiba will continue to satisfy market demand and to advance CMR drive data densities with MAMR technology.
MN09 is engineered for 24/7 operation and has a workload rating of 180TB/year [2]. Up to eight drive bays are supported by the NAS 3.5-inch [3] drive.
The 7200RPM 18TB NAS drive is designed with a 512MB buffer and delivers a consistent high level of performance with a sustained transfer rate of 268 MiB/s [4], making it the preferred choice of home offices and small businesses. The MN09 18TB is available now.
For more information on the new products, visit:
For more information on Toshiba’s full line of HDD storage products, visit:
Toshiba Electronic Devices & Storage Corporation
To learn more about our storage solutions visit the storage blog at Welcome to the Toshiba Storage Blog
[1] Definition of capacity: One terabyte (TB) = one trillion bytes, but storage capacity actually available may vary depending on operating environment and formatting. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
[2] Workload is a measure of the data throughput in a year, and it is defined as the amount of data written, read or verified by commands from the host system.
[3] "3.5-inch" means the form factor of HDDs. It does not indicate a drive's physical size.
[4] A mebibyte (MiB) means 220, or 1 048 576 bytes, and a gibibyte (GiB) means 230, or 1 073 741 824 bytes.
Product Inquiries:
Toshiba Electronic Devices & Storage Corporation
Storage Products Division
* FC-MAMRTM is a trademark of Toshiba Electronic Devices & Storage Corporation.
* Other company names, product names, and service names mentioned herein may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current and believed to be accurate as of the date of the announcement, but is subject to change without prior notice.