require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
March 31, 2022
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched a 150V N-channel power MOSFET “TPH9R00CQH” that uses the latest generation[1] process, “U-MOSX-H,” and that is suitable for use in switching power supplies for industrial equipment—including those deployed in data centers and communications base stations. Shipments start today.
TPH9R00CQH has a drain-source On-resistance about 42% lower than TPH1500CNH, a 150V product that uses the current generation process, U-MOSⅧ-H. Optimization of the new MOSFET’s structure has improved the trade-off[3] between the drain-source On-resistance and two charge characteristics[2], realizing excellent low-loss characteristics. In addition, spike voltage between the drain and source at switching operation is reduced, helping to lower electromagnetic interference (EMI) in switching power supplies. Two types of surface mount packages are available: SOP Advance and the more popular SOP Advance(N).
Toshiba also offers tools that support circuit design for switching power supplies. Alongside the G0 SPICE model, which can verify the circuit function in a short time, the highly accurate G2 SPICE models, which accurately reproduce transient characteristics, are now available.
Toshiba will expand its lineup of power MOSFETs that improve equipment power supply efficiency by cutting losses, helping to reduce power consumption.
Notes:
[1] Toshiba survey as of March 2022.
[2] Gate switch charge and output charge
[3] The product has improved the drain-source On-resistance x gate switch charge by about 20% and the drain-source On-resistance x output charge by about 28% compared to the current product TPH1500CNH (U-MOSⅧ-H series).
(Unless otherwise specified, @Ta=25°C)
Part number |
||||
---|---|---|---|---|
Absolute maximum ratings |
Drain-source voltage VDSS (V) |
150 |
||
Drain current (DC) ID (A) |
@Tc=25°C |
64 |
||
Channel temperature Tch (°C) |
175 |
|||
Electrical characteristics |
Drain-source On-resistance RDS(ON) max (mΩ) |
@VGS=10V |
9.0 |
|
@VGS=8V |
11 |
|||
Total gate charge (gate-source plus gate-drain) Qg typ. (nC) |
44 |
|||
Gate switch charge Qsw typ. (nC) |
11.7 |
|||
Output charge Qoss typ. (nC) |
87 |
|||
Input capacitance Ciss typ. (pF) |
3500 |
|||
Packages |
Name |
SOP Advance |
SOP Advance(N) |
|
Size typ. (mm) |
5.0×6.0 |
4.9×6.1 |
||
Sample Check & Availability |
Follow the link below for more on the new product.
Follow the link below for more on Toshiba MOSFETs.
Follow the link below for more on the highly accurate SPICE models(G2 model).
To check availability of the new product at online distributors, please visit:
Customer Inquiries
Power Device Sales & Marketing Dept.
Tel: +81-44-548-2216
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.