August 28, 2025
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan– Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched three 650V silicon carbide (SiC) MOSFETs equipped with its latest[1] 3rd generation SiC MOSFET chips and housed in surface-mount TOLL packages. The new devices are suitable for industrial equipment, such as switched-mode power supplies and power conditioners for photovoltaic generators. Volume shipments of the MOSFETs, “TW027U65C,” “TW048U65C,” and “TW083U65C,” start today.
The new products are Toshiba’s 3rd generation SiC MOSFETs in a general-purpose surface-mount TOLL package, which reduces device volume by more than 80% compared to through-hole packages such as TO-247 and TO-247-4L(X), and improves equipment power density.
The TOLL package also offers lower parasitic impedance[2] than through-hole packages, which helps to reduce switching losses. As a 4-terminal[3] package, a Kelvin connection can be used as the signal source terminal for the gate drive. This reduces the influence of inductance in the source wire within the package, achieving high-speed switching performance; in the case of TW048U65C, turn-on loss and turn-off loss are approximately 55% and 25%[4] lower, respectively, than in current Toshiba products[5], which will contribute to lower equipment power loss.
Toshiba will continue to expand its lineup to contribute to improved equipment efficiency and increased power capacity.
| Type | Package |
|---|---|
| Through-hole type | TO-247 |
| TO-247-4L(X) | |
| Surface-mount type | DFN8×8 |
| TOLL |
Measurement condition: VDD=400V, VGS=18V/0V, ID=20A, Ta=25°C, L=100μH, Rg (external gate resistor) =4.7Ω
The freewheeling diode uses the diode between the source and drain of each product.
(Toshiba comparison, as of August 2025)
Figure 1. Comparison of turn-on loss (Eon) and turn-off loss (Eoff) between TO-247 and TOLL package
Notes:
[1] As of August 2025.
[2] Resistance, inductance, etc.
[3] A product with a signal-source terminal connected close to the FET chip.
[4] As of August 2025, values measured by Toshiba. Please refer to Figure 1.
[5] A 650V 3rd generation SiC MOSFET with equivalent voltage and On-resistance that uses the TO-247 package without Kelvin connection.
(Unless otherwise specified, Ta=25°C)
| Part number | TW027U65C | TW048U65C | TW083U65C | |||
|---|---|---|---|---|---|---|
| Package | Name | TOLL | ||||
| Size (mm) | Typ. | 9.9×11.68×2.3 | ||||
| Absolute maximum ratings |
Drain-source voltage VDSS (V) | 650 | ||||
| Gate-source voltage VGSS (V) | -10 to 25 | |||||
| Drain current (DC) ID (A) | Tc=25°C | 57 | 39 | 28 | ||
| Electrical charac- teristics |
Drain-Source On-resistance RDS(ON) (mΩ) | VGS=18V | Typ. | 27 | 48 | 83 |
| Gate threshold voltage Vth (V) | VDS=10V | 3.0 to 5.0 | ||||
| Total gate charge Qg (nC) | VGS=18V | Typ. | 65 | 41 | 28 | |
| Gate-drain charge Qgd (nC) | VGS=18V | Typ. | 10 | 6.2 | 3.9 | |
| Input capacitance Ciss (pF) | VDS=400V | Typ. | 2288 | 1362 | 873 | |
| Diode forward voltage VDSF (V) | VGS=-5V | Typ. | -1.35 | |||
| Sample Check & Availability | ![]() |
![]() |
![]() |
|||
Follow the link below for more on Toshiba’s SiC Power Devices.
SiC Power Devices
Customer Inquiries:
Power & Small Signal Device Sales & Marketing Dept.
Tel: +81-44-548-2216
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.