This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Location of bottom mounting holes is different as following figure 1 and 2.
Note:
SFF-8301 specification from the industry-standard Small Form Factor (SFF) committee defines the dimensions for 3.5 inch Form Factor Disk Drives.
SFF-8301 defines three pairs of bottom mounting holes as follows:
Source: SFF Committee, SFF-8301 Specification for Form Factor of 3.5" Disk Drives Rev 1.6
March 16, 2010
"The pair of bottom mounting holes located by dimension A7 is required. One additional pair of bottom mounting holes are required, either the pair of mounting holes located by dimension A6 or the pair of mounting holes located by dimension A13. Providing all three pairs of mounting holes (located by dimensions A7, A6 and A13) is allowed."