This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
In most cases, rattling noises are normal and are no reason to worry. They are caused by mechanical parts of the HDD and just indicate that the drive is reading, writing or calibrating itself. Even if the drive is not being actively written to or read from, most operating systems do a lot of accesses to the system disk in the background. So if there is no additional indication for a defect, just the noise alone basically does not indicate that the drive is faulty. And Toshiba might recommend you to consult PC/system vendors or the shop you purchased the device/system about the phenomenon since the HDD is just a part of the system.