require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
11th February 2020
Reference system offers quick start for targeting accurate, power-optimized servo motor control
Toshiba Electronics Europe (“Toshiba”) today announced that they will launch their modular Servo Drive Reference Model (RM) Multi-Channel Motor Control reference platform at this year’s Embedded World exhibition under the banner of “The Journey of Motor Control”. This platform supports the growing interest in Industry 4.0 solutions where servo motors are integrated into applications such as collaborative robots (cobot). It also targets applications focused on accurate, energy efficient control, such battery powered lawn mowers, and 3D and additive printing technologies.
At the centre of the Servo Drive RM platform lies an Arm® Cortex®-M4 processor with FPU core-based microcontroller from Toshiba on an exchangeable plug-in card. This features an Advanced Vector Engine peripheral. Thanks to the Advanced Vector Engine implementing vector mathematics in hardware, together with its tight coupling with the analog-to-digital converter (ADC), the Programmable Motor Drive (PMD), and the Encoder (ENC) block, the load on the CPU is significantly reduced in motor control applications. Not only does this leave plenty of performance for other tasks, it also significantly reduces the engineering time required to implement vector motor control firmware.
The base platform is extendable, providing connectors for up to three power stages as well as an Arduino compliant interface communication to a host system can be realized via Arduino boards, CAN, Ethernet or even via the on-board Bluetooth 5 module
A low voltage power stage supporting brushless-DC (BLDC) motors requiring up to 48V and operating between 20W and 200W is also available. Featuring six TPW3R70APL MOSFETS utilizing the latest generation U-MOS IX-H silicon process, they feature an RDS(ON) of 3.7mΩ and support power dissipation of up to 170W. They are implemented in compact 5.0 x 6.0 x 0.73mm DSOP Advance, dual-side cooling packages. A range of encoder boards provide adaption to a cross-section of motor rotor encoders and resolvers.
Also, on display will be the software package that operates in conjunction with the Toshiba microcontroller and Servo Drive RM platform. Communicating via the system’s USB interface, it simplifies the configuration of the Advanced Vector Engine peripheral for optimum motor efficiency and control.
The Servo Drive RM provides a flexible and extendable reference platform for those involved in creating motor drive solutions that focus on accurate and energy efficient control. Additionally, Toshiba will be exhibiting a cross section of their other motor and stepper motor control solutions at the exhibition as part of the Journey of Motor Control.
The Toshiba stand is to be found in Hall 3A at stand 420.
Note:
* Arm and Cortex are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
* All other company names, product names, and service names mentioned herein may be trademarks of their respective companies.