require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
24th February 2022
Toshiba Electronics Europe GmbH (“Toshiba”) has launched an ultra-low capacitance TVS diode. The product will perform a useful function in protecting electronic components such as semiconductors from static electricity and noise while suppressing signal quality deterioration within high-frequency antennas used for electronic equipment. As such, the new product will be used in a wide range of electronic equipment, including mobile devices.
The new DF2B6M4BSL TVS diode features a total capacitance of just 0.12pF (0.15pF max.), which is the lowest for any such Toshiba device, representing an (approximate) 25% reduction in capacitance when compared to the existing Toshiba product (DF2B6M4ASL).
Within high-frequency antennas for radio communications such as Wi-Fi, the original signal quality must be kept, by avoiding any harmonic distortion caused by the added TVS diode capacitance. The new DF2B6M4BSL with its ultra-low capacitance shows a very fast response in suppressing high voltage spikes without affecting the original data signal quality.
When the DF2B6M4BSL is used at 5.0GHz, a common frequency in Wi-Fi applications, with a 20dBm input, the second harmonic is -64.7dB while the third is -55.5dB. The device is therefore suitable for ESD protection of high-frequency antennas.
Shipment of the new device starts today.