require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
08th February 2022
Toshiba Electronics Europe GmbH (“Toshiba”) has launched a three-phase brushless DC (BLDC) motor control pre-driver IC for motors that require high rotation speeds, such as those used for server fans, pumps, blowers and suction motors for cordless and robotic vacuum cleaners.
Toshiba’s new TC78B011FTG incorporates a sine-wave drive method reducing vibration and noise. Its sensorless design saves the space and cost of a Hall sensor. The built-in closed loop speed control regulates and maintains the motor’s rotational speed during dynamic power supply fluctuations and load variations without requiring an external microcontroller (MCU). Precise setting of a speed profile can be programmed into the built-in non-volatile memory (NVM).
Operating from a supply voltage ranging from 5.5 to 27V, the feature-rich device includes selectable closed loop or open loop speed control. Speed can either be controlled through a PWM signal, analog voltage or via the I²C interface. The I2C interface is also used to control various settings within the device. A standby function further improves overall system efficiency.
The TC78B011FTG is packaged in a P-WQFN36-0505-0.50-001 package with a footprint of just 5mm x 5mm and a height of 0.8mm.
Also available is Toshiba’s existing TC78B009FTG device, which uses trapezoidal control, allowing designers to select the most appropriate product depending on their preferred motor drive method.
Mass production and shipment of the TC78B011FTG starts today.