require 3 characters or more.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
30th August 2022
Toshiba Electronics Europe GmbH (“Toshiba”) has launched a total of five new third-generation 650V silicon carbide (SiC) MOSFET devices for industrial equipment.
These highly efficient and versatile products will be used in a variety of demanding applications including switch mode power supplies (SMPS) and uninterruptible power supplies (UPSs) for servers, data centers and communication equipment. They will also find applications in renewable energy, including photovoltaic (PV) inverters and bi-directional DC-DC converters, such as those used for electric vehicle (EV) charging.
The new TW015N65C, TW027N65C, TW048N65C, TW083N65C and TW107N65C are based upon Toshiba’s advanced third generation SiC process which optimizes the
cell structures used in second-generation devices.
As a result of this advancement, a key figure of merit (FoM) calculated as the product of drain-source on-resistance (RDS(on)) and gate-drain charge (Qg) to represent both static and dynamic losses has improved by about 80%. This significantly reduces losses and allows power solutions with higher power densities and lower running costs to be developed.
In common with earlier devices, the new third-generation MOSFETs include a built-in SiC Schottky barrier with a low forward voltage (VF) of -1.35V (typ.) to suppress fluctuation in RDS(on), thereby enhancing reliability.
The new devices are able to handle currents (ID) up to 100A and feature RDS(on) values as low as 15mΩ. All devices are housed in an industry standard TO-247 package.
Shipments of the new MOSFETs starts today.