Toshiba now sampling automotive gate driver IC for brushless DC motors

Cost-optimised gate driver supporting single shunt measurement

28th November 2024

Toshiba now sampling automotive gate driver IC for brushless DC motors

Düsseldorf, Germany, 28th November 2024 – Toshiba Electronics Europe GmbH (“Toshiba”) now provides engineering samples of its TB9084FTG, a MOSFET gate driver IC for three-phase brushless DC (BLDC) motors with a power rating of several hundred watts. The new device supports the trend of automotive OEMs replacing brushed DC motors with quieter, longer-lasting BLDC motors to drive body system applications like powered sliding passenger doors, power tailgates, and adjustable seats. The device can also drive BLDC motors to enhance the power performance of electric pumps and fans.

The main functions of the gate driver IC that were optimised include the 6-channel gate-driver structure, the additional gate-driver output to control the external MOSFET for reverse polarity protection, and the operational amplifier for one-channel motor current sensing, SPI communication, and the motor emergency stop function. Protection circuitry includes power supply under-voltage detection, charge pump overvoltage detection, thermal shutdown, and MOSFET drain-source voltage (VDS) monitoring.

The TB9084FTG is housed in a compact P-VQFN36-0606-0.50 package, measuring just 6mm×6mm, contributing to the miniaturisation of equipment. The operating temperature range is from -40 to +150°C, and the IC conforms to the AEC-Q100 (Grade 0) qualification. In addition, this package features a wettable flank structure, which facilitates automated optical inspection (AOI) to ensure the solder joint reliability.

Toshiba will further expand its lineup of gate driver ICs by optimising product functions based on market research. The company will continue to introduce new products to the market and contribute to the electrification and safety improvement of automotive equipment.

* SmartMCD™ is a trademark of Toshiba Electronic Devices & Storage Corporation.
* Other company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

A new window will open