Products that Contribute to Resolving Social Issues

We develop and provide products that consume less electricity when they are used and are smaller and lighter to achieve energy saving and greenhouse gas reduction in the end products of customers who use these products. 

Visconti™ Series Image Recognition Processors

icon
Visconti™ Series Image Recognition Processors

Product outline

This is an image recognition processor for on-board vehicle applications that achieves both high performance and energy saving.

Useful points

Images captured by a camera is instantaneously identified and the driver is notified of any danger.

Contribution to the environment

contributes to energy saving and preventing climate change with its multi-core and exclusive image processing circuits. 

DTMOS VI Series Power Semiconductors

icon
DTMOS VI Series Power Semiconductors

Product outline

It adopts a process that reduces loss. 

Useful points

It suppresses heat generation and also enables the downsizing of on-board devices. 

Contribution to the environment

It contributes to the prevention of climate change by saving energy. 

U-MOS X-H series Power Semiconductor

icon
U-MOS X-H series Power Semiconductor
Product outline It adopts a loss-reducing process.
Useful points It reduces heat generation, and it also supports miniaturization of mounted devices.
Contribution to the environment It contributes to the prevention of climate change by sabing energy.

Photorelays

icon
Photorelays

Product outline

This is the relay applying semiconductors to respond to the large current.

Useful points

It consumes less electricity, is smaller, and has longer life than the mechanical relay.

Contribution to the environment

It contributes to the prevention of climate change by saving energy, and downsizing of the devices to be installed.

Automotive Brushed DC Motor Driver ICs TB9053FTG

icon
Automotive Brushed DC Motor Driver ICs TB9053FTG

Product outline

It controls motors such as electric power steering.

Useful points

It supports miniaturization of control equipment by adopting a small package.

Contribution to the environment

It contributes to improved fuel economy of the vehicle through power savings.

NL HDD filled with helium

icon
NL HDD filled with helium
Product outline

An HDD filled with helium, which has smaller molecules than that of air. 

Useful points

It is used for servers and so on and supports society’s information infrastructure.

Contribution to the environment

By filling with helium, the rotation resistance is reduced, saving energy and increasing the capacity. 

Silicon Nitride Substrate

icon
Silicon Nitride Substrate
Product outline

The circuit board has high electrical insulation and thermal conductivity.

Useful points

It is essential for insulation and heat dissipation of power semiconductors in hybrid vehicles, etc.

Contribution to the environment

It contributes to downsizing and increase in efficiency of control circuits, and improves fuel efficiency.

RENECAT®

icon
RENECAT<sup>®</sup>

Product outline

It is a photocatalytic deodorizer that also has a sterilizing effect.

Useful points

It is solid and does not evaporate, so its effect is long-lasting.

Contribution to the environment

It does not use electricity like ordinary air purifiers, contributing to energy-saving.

Magnetrons

icon
Magnetrons
Product outline

Microwave oven is essential to our daily lives. Microwaves are generated with a magnetron*, heating by vibrating molecules in the food. (* : A type of vacuum tube)

Useful points

We were the first in the world to commercialize a tube that boasts a long service life, high-efficiency, and low-noise. 

Contribution to the environment

Contributes to energy saving and prevention of climate change by efficiently generating microwaves.

Electron beam (EB) mask writers

icon
Electron beam (EB) mask writers
Product outline

This equipment manufactures photomasks, which are indispensable for the production of semiconductors.

Useful points

By drawing masks with an electron beam, it can be used for fine processes.

Contribution to the environment

High-performance semiconductors manufactured with state-of-the-art processes contribute to energy-saving.