인터페이스 브릿지 IC(Mobile Peripheral Devices)

Recently, the interface method between the main processor such as baseband and application processor and the peripheral equipment such as camera and LCD display is different, and an interface bridge that converts and connects different interfaces is required.
We provide peripheral devices such as MPD (Mobile Peripheral Devices) and IO expanders to expand the functions of the main processor as an interface bridge that supports video data transmission methods such as MIPI🄬, LVDS, DisplayPort™, HDMI🄬 Interface.

Lineup

Interface Bridge Lineup

Lineup
Display Interface Bridge ICs
Toshiba display interface bridge has various display interfaces to facilitate the design of feature-rich mobile equipment realizing superb picture quality.

MIPI®, DSI®, DPI℠, LVDS, DisplayPort™, RGB

Camera Interface Bridge ICs
The camera interface bridge enables high-speed transfer of camera image data to support today’s higher camera resolutions.

MIPI® CSI-2®

HDMI® Interface Bridge ICs
There are many applications that require conversion from High-Definition Multimedia Interface (HDMI® Interface) to other formats such as the MIPI ® interface specification. These applications include digital media adapters, smart monitors, set-top boxes, Smart TVs and more.

HDMI® Interface, MIPI®, DSI®, CSI-2®

I/O Expander ICs
I/O Expander can easily expand the functions such as GPIOs, Keypads, LED controls and timers to the exsiting systems.

GPIO, PWM, I2C

Technical topics

문의

기술 문의

문의

문의

자주 있는 문의

자주 있는 문의

* MIPI®, DSI®, CSI-2®, DPI℠ are trademarks, service marks, registered service marks of MIPI Alliance, Inc.
* The terms HDMI, HDMI High-Definition Multimedia Interface, HDMI Trade dress and the HDMI Logos are trademarks or registered trademarks of HDMI Licensing Administrator, Inc.
* VESA® and DisplayPort™ are trademarks, service marks, registered trademarks, and/or registered service marks owned by VESA.
* DisplayPort™ and the DisplayPort™ logo are trademarks owned by the Video Electronics Standards Association (VESA®) in the United States and other countries.
* Other company names, product names, and service names may be trademarks of their respective companies.

A new window will open