This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
온라인 회로 시뮬레이터
A MOSFET selection tool that allows circuit simulation on the web.
Operation verification can be easily performed without the hassle of building a simulation environment and downloading element models.
What are the power semiconductors that will create a carbon-neutral future?
We Toshiba Electronic Devices and Storage Corporation contribute to the realization of a future carbon neutral world. By realizing high-performance power semiconductors with the latest technology. By accelerating energy conservation in all types of electrical equipment.
EDA/CAD Model Library
Various simulation models and 3D/land pattern data that improve design performance, such as high-precision SPICE models and thermal simulation models, can be downloaded for free.
Simple Over Temperature Detection Solution for Your Electronic Devices
Thermoflagger™ in combination with PTC thermistors helps to configure a simple over temperature detection solution and saves power.
Toshiba GaN Power device balances performance and ease of use
The energy conservation is attracting attention toward the realization of a carbon-free society, on the other hand, the demand for electric power continues to escalate. The need for highly efficient and compact electric power conversion systems increases rapidly. Not only improving the performance of Si power semiconductors, but also compound power semiconductors is introduced.
Next-generation power electronics opened up by Toshiba SiC devices
Toshiba advances SiC technologies for next-generation power electronics, and contributes to energy-saving society.
We provide reference designs that support device selection and optimal circuit solutions for highly efficient development and design approaches. Not only schematics as reference circuit but also PCB pattern data, Gerber data, and sample software as reference design are available for quick advancement of equipment designs. We hope these reference designs can be used as a base for new designs and support turn-key development which helps in reducing labor.