May 14, 2020
Toshiba Electronic Devices & Storage Corporation
TOKYO— Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has launched “TPD7107F,” a gate driver switch IPD[1] that controls the conduction and shut-off of current supplied to automotive electronic control units (ECUs), such as junction boxes and body control modules. Shipments start today.
Combined with Toshiba’s automotive low On-resistance N-channel MOSFET[2], TPD7107F can form a high-side switch suitable for load current. As an electronic switch, free from the contact wear of mechanical relays, the new IPD can help to reduce the size and power consumption of automotive ECUs, and to make them maintenance-free.
By delivering enhanced functions that support the high reliability required for automotive ECUs—a self-protection function and various built-in diagnostic functions that are output to the microcontroller—the new IPD monitors load operation and the MOSFET to which it is connected. In abnormal operation, it rapidly turns off the MOSFET[3] to reduce the load on the MOSFET.
TPD7107F is housed in a WSON10A[4] package, and it reduces peripherals such as capacitors since it has built in a voltage boosting circuit. The new IPD secures supply current as low as 3μA (max.) during stand-by.
Automotive equipment
(Unless otherwise specified, @Ta=25℃)
Part number |
|||||
|---|---|---|---|---|---|
Package |
WSON10A |
||||
Absolute maximum ratings |
Supply voltage VDD(1) (V) |
-16 to +26 |
|||
Supply voltage VDD(2) (V) |
@t≤400ms |
-36 to +36 |
|||
Supply voltage VD(3) (V) |
@t≤20ms |
-40 to +40 |
|||
Input voltage VIN(1) (V) |
-16 to +26 |
||||
Input voltage VIN(2) (V) |
@t≤400ms |
-36 to +36 |
|||
Input voltage VIN(3) (V) |
@t≤20ms |
-40 to +40 |
|||
Output source current IGATE(+) (mA) |
Internal capacity |
||||
Output sink current IGATE(-) (mA) |
5 |
||||
Power dissipation PD (W) |
1.84 |
||||
Operating temperature Topr (℃) |
-40 to +125 |
||||
Operating range |
Operating supply voltage VDD (V) |
@Tj= -40 to +125℃ |
5.75 to 26.00 |
||
Notes:
[1] IPD (Intelligent Power Device)
[2] Example of compatible devices: TPHR7904PB (40V/150A), TPH1R104PB (40V/120A)
[3] Rapid off state current (typ.): 237mA
[4] WSON10A: 3.0x3.0mm (typ.)
Follow the link below for more on the new product.
Follow the link below for more on Toshiba Automotive driver ICs.
*Company names, product names, and service names may be trademarks of their respective companies.
Customer Inquiries:
Power Device Sales & Marketing Department
Tel: +81-3-3457-3933
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.