February 9, 2022
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has released “TCK421G” for 20V power lines as the first product in its new “TCK42xG Series” of MOSFET gate driver ICs. Devices in the series are dedicated to gate voltage control of an external N-channel MOSFET, based on input voltage, and have an overvoltage lockout function. Volume shipments start today.
TCK421G is suitable for configuring power multiplexer circuits or load switch circuits equipped with reverse-current blocking, in combination with a back-to-back connection of external N-channel MOSFETs. It incorporates a charge pump circuit that supports a wide range of input voltages, from 2.7V to 28V, and supplies stable voltage to the gate-source voltage of external MOSFETs with its intermittent operation. This allows switching of large currents.
Housed in a WCSP6G[1] package, one of the smallest in the industry[2], TCK421G realizes high density mounting in small devices, such as wearable devices and smartphones, helping to reduce their footprint.
Toshiba will continue to develop the TCK42xG Series and plans to introduce six versions in all. The overvoltage lockout of TCK42xG Series will support an input voltage of 5V to 24V. Two types of gate output voltage, 5.6V and 10V, will be made available, for different gate-source voltages in the external MOSFETs. The overvoltage lockout and gate output voltage can be selected, according to the user’s device.
Notes:
[1] 1.2mm x 0.8mm
[2] Among MOSFET gate driver ICs. Toshiba survey, as of February 2022.
(Unless otherwise specified, Ta=25°C)
Part number |
|||
|---|---|---|---|
Package |
Name |
WCSP6G |
|
Size (mm) |
1.2×0.8 (typ.)、 t=0.35 (max) |
||
Operating ranges |
Input voltage VIN (V) |
@Ta= -40 to 85°C |
2.7 to 28 |
Electrical characteristics |
VIN UVLO threshold, Vout falling VIN_UVLO typ./max (V) |
@Ta= -40 to 85°C for VIN_UVLO max |
2.0/2.5 |
VIN UVLO hysteresis VIN_UVhyst typ. (V) |
– |
0.2 |
|
VIN OVLO threshold, Vout falling VIN_OVLO min/max (V) |
@Ta= -40 to 85°C |
22.34/24.05 |
|
VIN OVLO hysteresis VIN_OVhyst typ. (V) |
– |
0.12 |
|
Input quiescent current (ON state) [3] IQ(ON) typ. (μA) |
@VIN=5V |
140 |
|
@VIN=12V |
185 |
||
Standby current (OFF state) IQ(OFF) max (μA) |
@VIN=5V, Ta= -40 to 85°C |
0.5 |
|
@VIN=12V, Ta= -40 to 85°C |
0.9 |
||
GATE Drive voltage (VGATE1-VIN) (VGATE2-VIN) VGS min/typ./max (V) |
@VIN=2.7V |
8/9.2/10 |
|
@VIN=5V |
9/10/11 |
||
@VIN=9V |
9/10/11 |
||
@VIN=12V |
9/10/11 |
||
@VIN=20V |
9/10/11 |
||
VGS ON time tON typ. (ms) |
@VIN=5V, CGATE1,2=4000pF |
2.9 |
|
VGS OFF time tOFF typ. (μs) |
VIN=5V, @CGATE1,2=4000pF |
52 |
|
OVLO VGS turn OFF time tOVP typ. (μs) |
@CGATE1,2=4000pF |
34 |
|
Sample Check & Availability |
|||
Notes :
[3] Control terminal current (ICT) is not included.
Follow the links below for more on the new product.
To check availability of the new product at online distributors, visit:
Customer Inquiries
Small Signal Device Sales & Marketing Dept.
Tel: +81-44-548-2215
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.