September 25, 2025
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched “TPH2R70AR5,” a 100V N-channel power MOSFET fabricated with U-MOS11-H, Toshiba’s latest-generation process[1]. The MOSFET targets applications such as switched-mode power supplies for industrial equipment used in data centers and communications base stations. Shipments start today.
The 100V U-MOS11-H series improves on the drain-source On-resistance (RDS(ON)), total gate charge (Qg) and the trade-off between them (RDS(ON)×Qg) delivered by Toshiba’s existing generation process, the U-MOSX-H series, reducing both conduction and switching power losses.
TPH2R70AR5 offers approximately 8% lower RDS(ON) and 37% lower Qg against TPH3R10AQM, a U-MOSX-H series product, plus a 42% improvement in RDS(ON)×Qg. It also achieves high-speed body diode performance through the application of lifetime control technology[2], which reduces reverse recovery charge (Qrr) and suppresses spike voltage. Qrr is improved by approximately 38% and the RDS(ON)×Qrr is also improved by approximately 43%. These industry-leading[3] trade-off characteristics[4], both RDS(ON)×Qg and RDS(ON)×Qrr, minimize power loss, contributing to higher efficiency and power density in power supply systems. It also adopts the SOP Advance(N) package and offers excellent mounting compatibility with industry standards.
Toshiba also offers circuit design support tools: the G0 SPICE model, which verifies circuit function in a short time; and highly accurate G2 SPICE model that accurately reproduces transient characteristics. All are now available.
Toshiba will continue to expand its lineup of low-loss MOSFETs that enable more efficient power supplies and contribute to lower equipment power consumption.
Notes:
[1] As of September 2025, among Toshiba’s process technologies for low-voltage power MOSFETs. Toshiba survey.
[2] Lifetime control technology: Intentionally shortening the carrier lifetime by using the Pt diffusion process to introduce defects into the semiconductor enhances switching speed, which improves the recovery speed of the diode and reduces noise.
[3] As of September 2025, comparison with other 100V N-channel power MOSFETs for industrial equipment. Toshiba survey.
[4] RDS(ON)×Qg,: 120mΩ・nC (typ), RDS(ON)×Qrr: 127mΩ・nC (typ)
Revised, October 2, 2025.
“an ion beam” in note [2] has been corrected to “the Pt diffusion process.”
(Unless otherwise specified, Ta=25°C)
Part number | TPH2R70AR5 | |||
---|---|---|---|---|
Absolute maximum ratings | Drain-source voltage VDSS (V) | 100 | ||
Drain current (DC) ID (A) | Tc=25°C | 190 | ||
Channel temperature Tch (°C) | 175 | |||
Electrical characteristics |
Drain-source On-resistance RDS(ON) (mΩ) |
VGS=10V, ID=50A | Max | 2.7 |
VGS=8V, ID=50A | Max | 3.6 | ||
Total gate charge Qg (nC) | VDD=50V, VGS=10V, ID=50A | Typ. | 52 | |
Gate switch charge Qsw (nC) | Typ. | 17 | ||
Output charge Qoss (nC) | VDD=50V, VGS=0V, f=1MHz | Typ. | 106 | |
Input capacitance Ciss (pF) | VDS=50V, VGS=0V, f=1MHz | Typ. | 4105 | |
Reverse recovery charge Qrr (nC) | IDR=50A, VGS=0V, -dIDR/dt=100A/μs |
Typ. | 55 | |
Package | Name | SOP Advance(N) | ||
Size (mm) | Typ. | 5.15×6.1 | ||
Sample Check & Availability | ![]() |
Follow the link below for more on the new product.
TPH2R70AR5
Follow the link below for more on Toshiba’s MOSFETs.
MOSFETs
Follow the link below for more on the highly accurate SPICE models (G2 model).
G2 model
Customer Inquiries:
Power & Small Signal Device Sales & Marketing Dept.
Tel: +81-44-548-2216
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.