Toshiba Launches 100V N-Channel Power MOSFET with Its Latest Generation Process Technology[1] to Improve Efficiency in Switched-Mode Power Supplies for Industrial Equipment (Corrected, Oct. 2)

September 25, 2025

Toshiba Electronic Devices & Storage Corporation

Toshiba Launches 100V N-Channel Power MOSFET with the Latest Generation Process Technology to Improve Efficiency in Switched-Mode Power Supplies for Industrial Equipment

KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched “TPH2R70AR5,” a 100V N-channel power MOSFET fabricated with U-MOS11-H, Toshiba’s latest-generation process[1]. The MOSFET targets applications such as switched-mode power supplies for industrial equipment used in data centers and communications base stations. Shipments start today.

The 100V U-MOS11-H series improves on the drain-source On-resistance (RDS(ON)), total gate charge (Qg) and the trade-off between them (RDS(ON)×Qg) delivered by Toshiba’s existing generation process, the U-MOSX-H series, reducing both conduction and switching power losses.

TPH2R70AR5 offers approximately 8% lower RDS(ON) and 37% lower Qg against TPH3R10AQM, a U-MOSX-H series product, plus a 42% improvement in RDS(ON)×Qg. It also achieves high-speed body diode performance through the application of lifetime control technology[2], which reduces reverse recovery charge (Qrr) and suppresses spike voltage. Qrr is improved by approximately 38% and the RDS(ON)×Qrr is also improved by approximately 43%. These industry-leading[3] trade-off characteristics[4], both RDS(ON)×Qg and RDS(ON)×Qrr, minimize power loss, contributing to higher efficiency and power density in power supply systems. It also adopts the SOP Advance(N) package and offers excellent mounting compatibility with industry standards.

Toshiba also offers circuit design support tools: the G0 SPICE model, which verifies circuit function in a short time; and highly accurate G2 SPICE model that accurately reproduces transient characteristics. All are now available.

Toshiba will continue to expand its lineup of low-loss MOSFETs that enable more efficient power supplies and contribute to lower equipment power consumption.

Notes:
[1] As of September 2025, among Toshiba’s process technologies for low-voltage power MOSFETs. Toshiba survey.
[2] Lifetime control technology: Intentionally shortening the carrier lifetime by using the Pt diffusion process to introduce defects into the semiconductor enhances switching speed, which improves the recovery speed of the diode and reduces noise.
[3] As of September 2025, comparison with other 100V N-channel power MOSFETs for industrial equipment. Toshiba survey.
[4] RDS(ON)×Qg,: 120mΩ・nC (typ), RDS(ON)×Qrr: 127mΩ・nC (typ) 
 

Revised, October 2, 2025.
“an ion beam” in note [2] has been corrected to “the Pt diffusion process.”

애플리케이션

  • Power supplies for industrial equipment used in data centers and communications base stations
  • Switched-mode power supplies (high efficiency DC-DC converters, etc.)

Features

  • Low drain-source On-resistance: RDS(ON)=2.7mΩ (max) (VGS=10V, ID=50A, Ta=25°C)
  • Low total gate charge: Qg=52nC (typ.) (VDD=50V, VGS=10V, ID=50A, Ta=25°C)
  • Low reverse recovery charge: Qrr=55nC (typ.) (IDR=50A, VGS=0V, -dIDR/dt=100A/μs, Ta=25°C)

Main Specifications

(Unless otherwise specified, Ta=25°C)

Part number TPH2R70AR5
Absolute maximum ratings Drain-source voltage VDSS (V) 100
Drain current (DC) ID (A) Tc=25°C 190
Channel temperature Tch (°C) 175
Electrical
characteristics
Drain-source On-resistance
RDS(ON) (mΩ)
VGS=10V, ID=50A Max 2.7
VGS=8V, ID=50A Max 3.6
Total gate charge Qg (nC) VDD=50V, VGS=10V, ID=50A Typ. 52
Gate switch charge Qsw (nC) Typ. 17
Output charge Qoss (nC) VDD=50V, VGS=0V, f=1MHz Typ. 106
Input capacitance Ciss (pF) VDS=50V, VGS=0V, f=1MHz Typ. 4105
Reverse recovery charge Qrr (nC) IDR=50A, VGS=0V,
-dIDR/dt=100A/μs
Typ. 55
Package Name SOP Advance(N)
Size (mm) Typ. 5.15×6.1
Sample Check & Availability Buy Online

Follow the link below for more on the new product.
TPH2R70AR5

Follow the link below for more on Toshiba’s MOSFETs.
MOSFETs

Follow the link below for more on the highly accurate SPICE models (G2 model).
G2 model

To check availability of the new products at online distributors, visit:
TPH2R70AR5
Buy Online

Customer Inquiries:

  Power & Small Signal Device Sales & Marketing Dept.

  Tel: +81-44-548-2216

* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

A new window will open