3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
TST started the back-end processes, the assembly and packaging of the small signal devices and photocouplers at its Thai plant in April 2013. The Thai plant will extend its product lines in the years ahead. Toshiba has continued and will continue to invest in the discrete device business, promoting it as one of its major semiconductor businesses.
Location: | Prachinburi Prefecture, Thailand |
---|---|
Site Area: | Approx. 135,000㎡ |
Floor area: | Approx. 40,000㎡ |
Start of plant construction | July, 2012 |
Start of mass production | April, 2013 (Start of shipment: May, 2013) |
Production item: | Discrete semiconductors (small signal devices, photocouplers) |