東芝推出可提高SiC (碳化矽)MOSFET可靠性

July 30, 2020

Toshiba Electronic Devices & Storage Corporation

東芝電子元件及儲存裝置株式會社(東芝)推出可提高SiC(碳化矽)MOSFET[1]可靠性的元件結構。相較於東芝的典型元件結構,MOSFET內嵌的SBD(肖特基勢壘二極體[2])可在抑制導通電阻增大的同時,將元件結構的可靠性提高10倍以上[3]。

功率元件是降低車輛以及工業設備和其它電氣設備能耗的重要元件,而SiC相較於有機矽可進一步提高電壓並降低損耗,因此業界普遍預期SiC將成為新一代的功率元件材料。雖然SiC目前主要用於車輛變頻器,預計往後的應用領域會涉及於工業設備的各種光伏發電系統(PPS)和電源管理系統(PMS)。

可靠性問題是目前SiC元件最大課題,其涉及位於功率MOSFET的電源與列車之間的PN結二極體[4]。PN結二極體的外施電壓使其帶電,造成導通電阻變化,進而有損元件的可靠性。東芝新推出的SBD內嵌式MOSFET元件結構正是此問題的剋星。

新結構中有一個與電池單元內的PN結二極體平行設置的SBD,可防止PN結二極體帶電。相較於PN結二極體,內嵌SBD的通態電壓更低,因此電流會通過內嵌SBD,進而抑制導通電阻變化和MOSFET可靠性下降等問題。

內嵌SBD的MOSFET現已投入實際應用,但僅限於3.3kV元件等高壓產品;其通常會使導通電阻升高至僅高壓產品能承受的一個電壓水準。東芝在調整各個元件參數後發現MOSFET中SBD的面積比是抑制導通電阻增大的關鍵因素。東芝不斷優化SBD比例,實現了1.2kV高可靠型SiC MOSFET。並計畫於今年八月下旬(2020/Aug)開始量產。

Note
[1] MOSFET: metal-oxide-semiconductor field-effect transistor
[2] Schottky barrier diode: A semiconductor diode formed by the junction of a semiconductor with a metal.
[3] Toshiba defines reliability as a change in on-resistance when a current is applied from the source to the drain of a device at a current density of 250 A/cm2 for 1,000 hours. On-resistance changes by as much as 43% for Toshiba’s typical MOSFET, but it changes by only 3% in an SBD-embedded MOSFET.
[4] PN diode: A diode formed by the pn junction between the source and drain.

SBD內嵌式MOSFET元件結構

The structure of SBD-embedded MOSFET

SBD內嵌式MOSFET可抑制導通電阻變化

SBD-embedded MOSFET can suppress a change in on-resistance

Customer Inquiries:

Power Device Sales & Marketing Department
Tel: +81-3-3457-3933

*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

開啟新視窗