Toshiba Launches 80V N-Channel Power MOSFET Using Its Latest Generation Process to Improve Efficiency in AI Data Centers

June 30, 2026

Toshiba Electronic Devices & Storage Corporation

 Toshiba Launches 80V N-Channel Power MOSFET Using Its Latest Generation Process to Improve Efficiency in AI Data Centers

KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched "TPM1R408RH," an 80V N-channel power MOSFET fabricated using U-MOS11-H, Toshiba’s latest-generation process[1]. The MOSFET targets applications such as switched-mode power supplies for industrial equipment used in AI data centers and communications base stations. Shipments start today.

The continuing expansion in AI processing has increased power demand in data centers, while advances in communications infrastructure have further intensified requirements for higher efficiency, smaller size (higher power density), and lower electromagnetic interference (EMI) in switched-mode power supplies. As power losses directly affect system power consumption, heat generation, and cooling load, it is important to deploy power semiconductors with characteristics that support a balanced reduction in conduction and switching losses and that contribute to overall system optimization, including improved EMI suppression, thermal design, and ease of mounting.

TPM1R408RH features an optimized device structure and realizes a drain-source On-resistance of 1.4mΩ (max)[2], approximately 26% lower than that of "TPM1R908QM," an 80V Toshiba product fabricated using Toshiba’s previous-generation U-MOS X-H process. It also improves the trade-off between drain-source On-resistance (RDS(ON)) and total gate charge (Qg), achieving approximately a 45% reduction in the figure of merit, RDS(ON)×Qg over TPM1R908QM. These characteristics represent industry-leading[3] levels of low power loss.

TPM1R408RH also suppresses spike voltage generated between the drain and source during switching, helping to reduce EMI in switched-mode power supplies. EMI suppression often requires rework in later stages of design, but suppressing the device-originated spikes helps to reduce the rework and simplify filter and snubber circuits.

The new product adopts the SOP Advance(E) package, which delivers approximately 65% lower package resistance and approximately 15% lower thermal resistance than Toshiba’s current SOP Advance(N) package. By suppressing heat generation and improving heat dissipation, the package supports higher output and more compact power supply designs.

Toshiba also offers tools that support circuit design for switching power supplies. Alongside the G0 SPICE model, which verifies circuit function in a short time, highly accurate G2 SPICE models, which accurately reproduce transient characteristics, are now available. An online circuit simulator on the Toshiba website allows users to easily verify circuit operation in a web browser, with no need to set up a simulation environment or download device models. (Online circuit simulator: here)

Toshiba will continue to expand its lineup of power MOSFETs that improve power supply efficiency, thereby helping to reduce power consumption in industrial equipment.

 

Figure 1. Reduction of drain-source On-resistance (comparison of Toshiba products)
Figure 1. Reduction of drain-source On-resistance (comparison of Toshiba products)
Figure 2. Reduction of drain-source On-resistance × total gate charge (comparison of Toshiba products)
Figure 2. Reduction of drain-source On-resistance × total gate charge (comparison of Toshiba products)

Notes:
[1] As of June 2026, based on Toshiba’s low-voltage power MOSFET processes.
[2] VGS=10V, ID=50A, Ta=25°C
[3] Toshiba survey, as of June 2026.

Applications

Industrial Equipment

  • Switched-mode power supplies for AI data centers and communications base stations

Features

  • Low drain-source On-resistance: RDS (ON)=1.4mΩ (max) (VGS=10V, ID=50A, Ta=25°C)
  • Low drain-source On-resistance × total gate charge: RDS (ON)×Qg=1.4mΩ×80nC=112mΩ・nC
    (approximately 45% lower than 1.9 mΩ×108nC=205.2 mΩ・nC for TPM1R908QM)
  • Adoption of the SOP Advance (E) package with low package resistance and low thermal resistance.

Main Specifications

(Unless otherwise specified, Ta=25°C)

Part number TPM1R408RH
Absolute maximum
ratings
Drain-source voltage VDSS (V) 80
Drain current (DC) ID (A) Tc=25°C 288
Channel temperature Tch (°C) 175
Electrical characteristics Drain-source On-resistance RDS(ON) (mΩ) VGS=10V Max 1.4
VGS=8V Max 1.7
Total gate charge Qg (nC) VGS=10V Typ. 80
Gate switch charge Qsw (nC) Typ. 23
Output charge Qoss (nC) Typ. 161
Reverse recovery time trr (ns) Typ. 74
Reverse recovery charge Qrr (nC) Typ. 115
Package Name SOP Advance(E)
Size (mm) Typ. 4.9×6.1×1.0
Sample Check & Availability Buy Online

Follow the link below for more on the new product.
TPM1R408RH

Follow the link below for more on Toshiba’s MOSFETs.
MOSFETs

To check availability of the new product at online distributors, visit:
TPM1R408RH
Buy Online

Customer Inquiries:

  Power & Small Signal Device Sales & Marketing Dept.

  Tel: 044-548-2216

* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.

A new window will open