※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
※ : Products list (parametric search)
This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Half-Bridge_Bridge-Rectification has been added to both the AC-DC and DC-DC converter sections.
A MOSFET Gate Drive Voltage adjustment function has been added.
A PCB Illustration Window has been added to the Totem-Pole_PFC and the Semi-Bridgeless_PFC topologies of the AC‑DC Converter.
A PCB Illustration Window has been added to the Single_PFC and the Interleaved_PFC sections of the AC DC converter.
An H‑Bridge for Brushed DC Motors and a 3‑Phase Inverter (SPMSM) for Brushless Motors have been added in New Motor Drive Circuit Simulation target topologies.
A Semi‑Bridgeless_PFC has also been added to the AC‑DC converter in the Power Supply Circuit Simulation target topologies.
A PCB Illustration Window has been added to the AC-DC and DC-DC Full-Bridge sections.
A Totem-Pole_PFC topology has been added to the AC-DC converter.
A PCB Illustration Window has been added to the AC-DC and DC-DC Half-Bridge sections.
A Interleaved_PFC topology has been added to the AC-DC converter.
A PCB Illustration Window has been added to the AC-DC and DC-DC Flyback, and the DC-DC Non-Isolated_Buck_Converter sections.
A Single_PFC topology has been added to the AC-DC converter.
The feature enabling arbitrary setting of transformer parameters has been added to the Full-Bridge circuit of the AC-DC/DC-DC converter.
A feature has been added to the AC-DC/DC-DC converter's half-bridge circuit, allowing the transformer parameters to be set arbitrarily.
A feature has been added to the AC-DC converter’s flyback circuit, allowing the transformer parameters to be set arbitrarily.
A feature has been added to the DC-DC converter's flyback circuit, allowing the transformer parameters to be set arbitrarily.
Three topologies (Flyback, Half-Bridge, Full-Bridge) have been added to the DC-DC converter for the second stage of AC-DC converter.
The Online Simulator allows users to verify and select MOSFETs.
Operation is easily verified without the hassle of building a simulation environment and downloading element models.
By changing the MOSFET and circuit constants and comparing the simulation result waveforms and power conversion efficiency, you can identify the MOSFET that matches the target specifications.
Login is required to use the circuit simulator.
* Simulation is recommended for use on a PC. System maintenance will take place every Tuesday from 8:00 AM to 10:00 AM (JST). During this period, the system may not operate normally.
| Power Supply Type | Topology | Input Voltage Range (V) | Output Power Range (W) | |
|---|---|---|---|---|
AC-DC |
PFC (First Stage of AC-DC) | Single_PFC | 100 or 230 | 400 to 1600 |
| Interleaved_PFC | 100 or 230 | 400 to 1600 | ||
| Totem-Pole_PFC | 100 or 230 | 400 to 1600 | ||
| Semi-Bridgeless_PFC | 100 or 230 | 400 to 1600 | ||
| DC-DC (Second Stage of AC-DC) | Flyback | 300 to 420 | 5 to 120 | |
| Half-Bridge | 300 to 420 | 100 to 1600 | ||
| Half-Bridge_Bridge-Rectification |
300 to 420 | 100 to 1600 | ||
| Full-Bridge | 300 to 420 | 300 to 2000 | ||
DC-DC |
Flyback | 12 to 100 | 1 to 120 | |
| Non-Isolated_Buck_Converter | 10 to 60 | 1 to 100 | ||
| Half-Bridge | 12 to 180 | 100 to 300 | ||
| Half-Bridge_Bridge-Rectification |
12 to 180 | 100 to 300 | ||
| Full-Bridge | 12 to 180 | 200 to 500 | ||
* Simulation is recommended for use on a PC. System maintenance will take place every Tuesday from 8:00 AM to 10:00 AM (JST). During this period, the system may not operate normally.
| Motor Type | Topology | Input Voltage Range(V) | Output Torque (mN*m) | |
|---|---|---|---|---|
| Motor Drive | Brushed_DC_Motor | H-Bridge | 9 to 48 | 10 to 500 |
| Brushless_Motor | 3-Phase_Inverter_SPMSM | 9 to 100 | 10 to 2000 | |
Note : SPMSM (Surface Permanent Magnet Synchronous Motor)