3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
Company about
December 3, 2019
Toshiba Electronic Devices & Storage Corporation
TOKYO — November 26, 2019 — Toshiba Electronic Devices & Storage Corporation (“Toshiba”) announces the DT02-V Series of Surveillance HDDs, its new series created for digital video recorder (DVR) and network video recorder (NVR) platforms.
The new series utilizes the latest magnetic recording technologies to achieve high areal density, helping to improve reliability compared to the prior MD04ABA-V Series. With up to 6TB capacity[1], the new DT02-V Series supports a maximum of 32 high-resolution camera streams[2] and is suitable for use in leading surveillance DVR and NVR platforms with as many as eight drive bays.
“Our latest surveillance HDD family, the DT02-V Series, delivers up to 6TB of storage capacity, and is designed for use with leading surveillance DVR and NVR platforms,” says Shuji Takaoka, General Manager of Storage Products Sales & Marketing Division at Toshiba Electronic Devices & Storage Corporation. “It also provides a variety of capacity options while improving reliability for high resolution surveillance video streams.”
The DT02-V Series is designed for robust 24/7 operation at HDD temperatures as high as 40ᵒC for 600,000 load/unload cycles, at rated workload[3] of 180TB a year. Other features include a SATA 6Gbit/s interface[4] with a 128MiB cache to help minimizing frame drops, and a robust mechanical platform designed to achieve a 1 million-hour MTTF[5].
The DT02-V Series 4TB samples are available from today, 6TB samples will be planned from Jan 2020, and a 2TB sample is expected to be available in March 2020.
For more information on the new products, please visit:
Notes:
[1] Definition of capacity: Toshiba defines a megabyte (MB) as 1 000 000 bytes, a gigabyte (GB) as 1 000 000 000 bytes and a terabyte (TB) as 1 000 000 000 000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1 073 741 824 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system, such as Microsoft Operating System and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
[2] Number of surveillance cameras support capability is defined by performance simulation with High Definition cameras at 4Mbit/s rate. Actual results may vary based on various factors, including the types of cameras installed, the system’s hardware and software capabilities, and the video compression technology used, as well as system variables such as resolution, frames per second, and other settings.
[3] Workload is a measure of the data throughout of the year, and it is defined as the amount of data written, read or verified by commands from the host system.
[4] Read and write speed may vary depending on the host device, read and write conditions, and file size.
[5] MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF.
* Information in this document, including product prices and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement but is subject to change without prior notice.
* Images displayed in the banners are for illustration purposes only and do not show the actual products. The images are merely intended to help illustrate the function of the products.
* Company names, product names, and service names may be trademarks of their respective companies.