Toshiba Adds Automotive Display Interface Bridge ICs for In-Vehicle Infotainment Systems

June 2, 2020

Toshiba Electronic Devices & Storage Corporation

TC9594XBG

TOKYO—Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has added “TC9594XBG” and “TC9595XBG,” new interface bridge ICs for automotive In-Vehicle Infotainment (IVI) systems, to its lineup of display interface bridge ICs. Sample shipments start this month.

Automotive IVI systems are becoming increasingly sophisticated, and as the number of displays they incorporate grows, so too do panel choices, moving beyond the widely used LVDS display. However, this can present a problem for current systems that do not support the interfaces of new display panels, including DSISM and eDP. The solution is found in interface bridge ICs.

Toshiba brings a wealth of experience to this market segment, gained from developing ICs supporting MIPI® interface for consumer applications. It has now added the following functions to its lineup for automotive applications, a move that solves interface difference problems in automotive systems and supports customers working on system designs.

 

TC9594XBG: Parallel to MIPI DSI
TC9595XBG: MIPI DSI /DPISM to DisplayPort

Key Features

 

TC9594XBG

TC9595XBG

Input

Parallel input

24-bit @ 166MHz

- MIPI DSI 4 Lanes x 1ch

- MIPI DPI 24bit@154MHz

Output

- MIPI DSI-TX

4 Lanes x 1ch

- VESA®

DisplayPort 1.1a

Resolution

WUXGA 1920 x1200 @ 24-bit

WUXGA 1920 x1200 @ 24-bit

Ta

- 40 to 105℃

- 40 to 85℃

Package

VFBGA80

7mm x 7mm, 0.65mm pitch

VFBGA80

7mm x 7mm, 0.65mm pitch

For more information on the new products, please visit:

TC9594XBG

TC9595XBG

*MIPI® is a registered trademark of MIPI Alliance, Inc. DPI and DSI are service marks of MIPI Alliance, Inc.
*DisplayPort and the DisplayPort logo are trademarks owned by the Video Electronics Standards Association (VESA®) in the United States and other countries.
*Other company names, product names, and service names may be trademarks of their respective companies.

Customer Inquiries:

System Devices Sales & Marketing Dept.

Tel: +81-3-3457-3332

Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.