3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
February 18, 2021
Toshiba Electronic Devices & Storage Corporation
Tokyo, Japan —February 18, 2021 —Toshiba Electronic Devices & Storage Corporation (Toshiba) announces the 18TB[1] MG09 Series HDD, Toshiba’s first HDD models with energy-assisted magnetic recording. The MG09 Series features Toshiba’s third-generation, 9-disk Helium-sealed design and Toshiba’s innovative Flux Control – Microwave Assisted Magnetic Recording (FC-MAMR) technology, to advance Conventional Magnetic Recording (CMR) density to 2TB per disk, achieving a total capacity of 18TB.
Sample shipments of 18TB MG09 Series HDD to customers are expected to start sequentially at the end of March 2021.
With 12.5% more capacity than prior 16TB models, 18TB MG09 CMR drives are compatible with the widest range of applications and operating systems. The MG09 are adapted to mixed random and sequential read and write workloads in both cloud-scale and traditional data center use cases. The MG09 features 7,200rpm performance, a 550TB per year workload rating[2], and a choice of SATA and SAS interfaces—all in a power-efficient Helium-sealed industry-standard, 3.5-inch[3] form factor.
The MG09 Series further illustrates Toshiba’s commitment to advancing HDD design to meet the evolving needs for storage devices in cloud-scale servers and Object and File storage infrastructure. With its improved power efficiency and 18TB capacity, the MG09 Series helps cloud-scale infrastructure advance storage density to reduce capex and improve TCO (total cost of ownership). As data growth continues at an explosive pace, advanced 18TB MG09 with FC-MAMR technology will help cloud-scale service providers and storage solution designers achieve higher storage densities for cloud, hybrid-cloud and on-premises rack-scale storage.
“Toshiba’s new 18TB MG09 Series delivers new levels of storage density and power efficiency to our cost-conscious cloud-scale and storage solutions customers. Our HDD technology is able to achieve our customers’ critical TCO objectives at a cost of pennies per GB,” said Shuji Takaoka, General Manager of the Storage Products Sales & Marketing Division at Toshiba Electronic Devices & Storage Corporation. “Our 3rd generation 9-disk Helium-sealed design provides a field-tested foundation for achieving a massive 18TB capacity. The addition of Toshiba’s innovative FC-MAMR technology advances CMR capacity to 18TB, delivering compatibility with the widest range of applications and operating environments.”
For more information on the new products, please visit:
For more information on Toshiba's full line of HDD storage products, visit:
[1] Definition of capacity: One terabyte (TB) = one trillion bytes, but storage capacity actually available may vary depending on operating environment and formatting. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
[2] Workload is a measure of the data throughput in a year, and it is defined as the amount of data written, read or verified by commands from the host system.
[3] "3.5-inch" means the form factor of HDDs. It does not indicate a drive's physical size.
Product Inquiries:
Toshiba Electronic Devices & Storage Corporation
Storage Products Division
* Information in this document, including product prices and specifications, content of services and contact information, is current and believed to be accurate as of the date of the announcement, but is subject to change without prior notice.
* Company names, product names, and service names mentioned herein may be trademarks of their respective companies.