August 21, 2025
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan–Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched an automotive photorelay[1], "TLX9161T," in a small SO12L-T package, that achieves an output withstand voltage of 1500V (min), the level required to support high voltage automotive batteries. Volume shipments start today.
Key challenges in popularizing electric vehicles include reducing charging times and improving cruising range. Addressing these requires efficient operation of the battery system. This is done by the battery management system (BMS), which monitors the battery’s charge status to enable high-efficiency system operation, and also monitors isolation between the battery and the vehicle body to ensure the safe use of high-voltage batteries. Electrically isolated photorelays are used in BMS that handle high voltages.
Toshiba’s new product, a high-voltage photorelay with an output withstand voltage of 1500V (min), is a miniaturized version of Toshiba's TLX9160T photorelay. Miniaturizing the TLX9160T’s built-in MOSFET chip has achieved integration into the SO12L-T package, which has a mounting area approximately 25%[2] smaller than the TLX9160T’s SO16L-T package. This size reduction also contributes to miniaturization and cost reduction of the BMS. The pin pitch and pin layout are the same (Figure 1) as those of the SO16L-T, enabling use of the same circuit board pattern design.
The new photorelay uses a resin with a Comparative Tracking Index (CTI[3]) exceeding 600, which is classified under Material Group I[4] of the IEC 60664-1[5] international standard. The pin configuration ensures a creepage distance of more than 5mm[6] on the detector side (Figure 2). This realizes compliance with IEC 60664-1, supporting an operating voltage of 1000V.
Toshiba will continue to expand its lineup of automotive photorelay products and provide solutions that address the challenges in popularizing electric vehicles, aiming to contribute to the realization of a carbon-neutral society.
Notes:
[1] Photorelay: The primary (control) and the secondary (switch) sides are electrically isolated. Switches connected directly to the AC line, and switches between equipment that differ in ground potential, can be controlled through insulating barriers.
[2] Comparison of SO16L-T package size (10.3×10.0×2.45mm) with SO12L-T package size (7.76×10.0×2.45mm).
[3] Comparative Tracking Index (CTI): An index that indicates the voltage withstand capability of an insulating material before an electrical track (conductive path) forms along its surface.
[4] Material Group I: A classification of molded materials in IEC 60664-1 that refers to materials with a Comparative Tracking Index (CTI[3]) of 600 and more.
[5] IEC 60664-1: The standard that specifies principles, requirements, and test methods for insulation coordination for systems up to AC 1000V or DC 1500V.
[6] More than 5mm: The required creepage distance for an operating voltage 1000V, material group I, pollution degree 2 (the degree of pollution of the operating environment where electrical equipment is used; pollutants are entirely non-conductive, but could potentially be rendered conductive by condensation.)
(Unless otherwise specified, Ta=25°C)
| Part number | TLX9161T | |||
|---|---|---|---|---|
| Contact | 1-Form-A | |||
| Absolute maximum ratings |
Input forward current IF (mA) | 30 | ||
| ON-state current ION (mA) | 30 | |||
| Operating temperature Topr (°C) | -40 to 125 | |||
| Avalanche current IAV (mA) | 0.6 | |||
| Electrical characteristics |
OFF-state current IOFF (nA) | VOFF=1000V | Max | 100 |
| Output withstand voltage VOFF (V) | IOFF=10μA | Min | 1500 | |
| Recommended operating conditions |
Supply voltage VDD (V) | Max | 1000 | |
| Coupled electrical characteristics |
Trigger LED current IFT (mA) | ION=30mA, t=10ms | Max | 3 |
| Return LED current IFC (mA) | IOFF=100μA, Ta=-40 to 125°C, t=40ms |
Min | 0.05 | |
| ON-state resistance RON (Ω) | ION=30mA, IF=10mA, t<1s |
Max | 500 | |
| Switching characteristics |
Turn-on time tON (ms) | IF=10mA, RL=20kΩ, VDD=40V |
Max | 1 |
| Turn-off time tOFF (ms) | Max | 1 | ||
| Isolation characteristics |
Isolation voltage BVS (Vrms) | AC, 60s | Min | 5000 |
| Clearance distance (mm) | Min | 8 | ||
| Creepage distance (mm) | Min | 8 | ||
| Package | Name | SO12L-T | ||
| Size (mm) | Typ. | 7.76×10.0×2.45 | ||
| Sample Check & Availability | ![]() |
|||
Follow the link below for more on the new product.
TLX9161T
Follow the link below for more on Toshiba’s Isolators and Solid State Relays.
Isolators/Solid State Relays
Follow the link below for more on Toshiba’s Automotive Devices.
Automotive Devices
Customer Inquiries:
Optoelectronic Device Sales & Marketing Dept.
Tel: +81-44-548-2218
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.