News Center

This page is listing links of the press release and topics published by Toshiba Electronic Devices and Storage Corporation.
Information in the news and topics, including product prices and specifications, content of services and contact information, is current on the date of the news announcement, but is subject to change without prior notice. The news before March 31, 2017 is the news published by Toshiba Storage & Electronic Devices Solutions Company.

Release Year
Category
News Category
22-01-2019
Toshiba Expands Ethernet Bridge IC Lineup for Automotive and Industrial Applications
08-01-2019
TOSHIBA 推出 16TB MG08 系列硬碟
07-01-2019
Toshiba Develops DNN Hardware IP for Image Recognition AI Processor Visconti™5 for Automotive Driver Assistance Systems
20-12-2018
A discrete IGBT with wide SOA for PFCs of air conditioners’ power supplies: GT50J123
19-12-2018
A TVS diode with an increased peak pulse current rating to improve surge protection performance for mobile devices: DF2B5BSL
13-12-2018
Consumption energy saving general-purpose rectifiers with high ESD protection ability: CRG09A, CRG10A
12-12-2018
Toshiba Launches H-bridge Driver IC Supporting 1.8V Low-Voltage and 4.0A Large-Current Drive
06-12-2018
TOSHIBA N300 NAS硬碟 推出全新12TB與14TB氦氣填充封裝機型
04-12-2018
TOSHIBA推出全新 4TB CANVIO 外接式硬碟 儲存個資更安全可靠
19-11-2018
Toshiba Testing Laboratory Meets Global Standard, Receive ISO/IEC 17025 Accreditation
13-11-2018
Toshiba Unveils 130nm FFSA™ Development Platform Featuring High Performance, Low Power and Low Cost Structured Array
31-10-2018
Toshiba Adds New 4-channel High-Efficiency Linear Power Amplifier for Car Audios Featuring Maximum 45W Output
30-10-2018
Toshiba Releases Bluetooth® 5 IC for Automotive Applications
03-10-2018
TVS diodes with improved electrostatic discharge protection performance for high-speed signal lines: DF2B5M5SL, DF2B6M5SL, DF2S5M5SL, DF2S6M5SL
28-09-2018
A small, low forward voltage Schottky barrier diode suitable for voltage booster circuits of LCD backlights: CLS10F40
27-09-2018
Toshiba has launched IPM-drive photocoupler in thin, compact 5pin SO6 package, helping downsizing equipment: TLP2304
26-09-2018
Toshiba Releases DC Brushed Motor Driver IC with Current Limiter Detection
25-09-2018
Toshiba Launches Power Amplifier for Car Audio with Strong Resistance to Power Surges
07-09-2018
Toshiba’s Advanced Bluetooth® Low Energy SoC Delivers Long-distance Communication in a Compact Module
06-09-2018
Toshiba Starts Mass Production of Motor Driver IC with High-Definition Micro Stepping
開啟新視窗