Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Announces Latest Ethernet Bridge IC for Automotive and Industrial applications

 January 21, 2019 

New IC Supports Time-Sensitive Networking Protocol and Ethernet Bridging Bandwidth up to 1Gbps

Toshiba TC9562

IRVINE, Calif. – Toshiba America Electronic Components, Inc. (“Toshiba”) today has announced TC9562 series, its latest member in the automotive network bridge IC product line. The TC9562 series provides advanced Ethernet capability for telematics and infotainment systems for the automotive segment.

Real-time processing and reliable data transmission is critical to support telematics, infotainment, driver assistance systems and various sensor data to enable a fully connected vehicle. New standards, including Ethernet AVB1 and TSN2, are becoming adopted in automotive and industrial applications to meet the increased performance requirements.

Toshiba’s TC9562 series is designed for reliability and performance delivering Ethernet bridging capability up to 1Gbps bandwidth. The new automotive bridge IC also supports Time-Sensitive Networking (TSN) protocol for various industrial and commercial applications.

The TC9562 series’s advanced capabilities supports Ethernet AVB specification, specifically IEEE 802.1AS3 and IEEE 802.1Qav4, as well as TSN standards IEEE 802.1Qbv5, IEEE 802.1Qbu6 and IEEE 802.3br6. The New IC also supports a broad range of interfaces including PCI Express® 2.0 and 1.0, I2S/TDM, RGMII, RMII, MII7 and an option for SGMII7 for expanded interfaces to various IVI SoC solutions.

“We had the pleasure of working with Toshiba to feature their Ethernet bridge IC solutions in our industry-leading Qualcomm® Snapdragon™ 820A Platform,” said Shyam Krishnamurthy, senior director of Qualcomm Technologies, Inc., “We look forward to continuing our combined efforts to design cutting-edge solutions to support highly advanced automotive cockpit and telematics applications.”

Shardul Kazi, Chief Marketing Officer at Toshiba America Electronic Components, Inc., commented, “We are pleased to expand the successful automotive Ethernet bridge IC series to the market. We hope to help accelerate the Ethernet adoption in automotive applications.”

The TC9562 series will be automotive qualified8 and packaged in P-LFBGA120 in 9mm x 9mm package. Sample shipments will start in February 2019, and volume production will start in October 2019. 

For further information and the detailed product specifications please visit:  https://toshiba.semicon-storage.com/us/product/automotive/interface-bridge.html.

About Toshiba America Electronic Components, Inc.

Toshiba America Electronic Components, Inc. (TAEC) an independent operating company owned by Toshiba America, Inc., is the US based electronic components business of Toshiba Electronic Devices and Storage Corporation. TAEC offers consumers and businesses a wide variety of innovative hard disk drive (HDD) products plus semiconductor solutions for automotive, industrial, IoT, motion control, telecoms, networking, consumer and white goods applications. The company’s broad portfolio encompasses integrated wireless ICs, power semiconductors, microcontrollers, optical semiconductors, ASICs, ASSPs and discrete devices ranging from diodes to logic ICs.  For more company information visit TAEC’s web site at http://www.toshiba.semicon-storage.com/

1 Ethernet AVB: IEEE802.1 Audio/Video Bridging
2 Ethernet TSN: IEEE802.1 Time Sensitive Networking
3 IEEE 802.1AS: Standard for time synchronization 
4 IEEE 802.1Qav: Standard for traffic shaping 
5 IEEE 802.1Qbv: Standard for Enhancements to scheduled traffic
6 IEEE 802.1Qbu/IEEE 802.3br: Standard for Frame preemption/Interspersing Express Traffic
7 SGMII, RGMII, RMII, MII: Ethernet interface. SGMII = Serial Gigabit Media Independent Interface; RGMII = Reduced Gigabit Media Independent Interface; RMII = Reduced Media Independent Interface; MII = Media Independent Interface
8 AEC: Automotive Electronics Council. The new bridge ICs will be AEC-Q100 grade 3 qualified

* Qualcomm and Snapdragon are trademarks of Qualcomm Incorporated, registered in the United States and other countries. Qualcomm Snapdragon is a product of Qualcomm Technologies, Inc. and/or its subsidiaries.
* Arm and Cortex are registered trademarks of Arm Limited (or one of its subsidiaries) in the United States or other countries.
* PCI Express and PCIe are registered trademarks of PCI-SIG.
* All other company names, product names and service names may be trademarks of their respective companies.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice.

A new window will open