Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba Releases MOSFET Gate Driver Switch IPD for Automotive ECUs

May 14, 2020

TPD7107F

TOKYO— Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has launched “TPD7107F,” a gate driver switch IPD[1] that controls the conduction and shut-off of current supplied to automotive electronic control units (ECUs), such as junction boxes and body control modules. Shipments start today.

Combined with Toshiba’s automotive low On-resistance N-channel MOSFET[2], TPD7107F can form a high-side switch suitable for load current. As an electronic switch, free from the contact wear of mechanical relays, the new IPD can help to reduce the size and power consumption of automotive ECUs, and to make them maintenance-free.

By delivering enhanced functions that support the high reliability required for automotive ECUs—a self-protection function and various built-in diagnostic functions that are output to the microcontroller—the new IPD monitors load operation and the MOSFET to which it is connected. In abnormal operation, it rapidly turns off the MOSFET[3] to reduce the load on the MOSFET.

TPD7107F is housed in a WSON10A[4] package, and it reduces peripherals such as capacitors since it has built in a voltage boosting circuit. The new IPD secures supply current as low as 3μA (max.) during stand-by.

Applications

Automotive equipment

  • ECUs (body control modules, junction boxes, etc.)
  • Power distribution modules
  • Semiconductor relays

Features

  • AEC-Q100 qualified
  • Can be used in combination with a low On-resistance N-channel MOSFET[2], depending on load current
  • Built-in voltage boosting circuit, reducing passive peripheral components
  • Built-in protection features and diagnostic output functions
    (voltage abnormalities, over current, over temperature, reverse connection of power supply, protection for disconnection of GND terminal, and VDD short of load line, etc.)

Follow the link below for more on the new product.

TPD7107F    

Follow the link below for more on Toshiba Automotive driver ICs.

Automotive driver ICs  

About Toshiba America Electronic Components, Inc.

Toshiba America Electronic Components, Inc. (TAEC), an independent operating company owned by Toshiba America, Inc., is the US based electronic components business of Toshiba Electronic Devices and Storage Corporation. TAEC offers a wide variety of innovative hard disk drive (HDD) products and semiconductor solutions for data center, automotive, industrial, IoT, motion control, telecom, networking, consumer, and white goods applications. The company’s broad portfolio encompasses enterprise and consumer HDDs integrated wireless ICs, power semiconductors, microcontrollers, optical semiconductors.

Notes:
[1] IPD (Intelligent Power Device)
[2] Example of compatible devices: TPHR7904PB (40V/150A), TPH1R104PB (40V/120A)
[3] Rapid off state current (typ.): 237mA
[4] WSON10A: 3.0x3.0mm (typ.)

*Company names, product names, and service names may be trademarks of their respective companies.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

A new window will open