Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

Toshiba and Japan Semiconductor Develop Technology to Improve Reliability of Pch-LDMOS for Analog ICs

September 23, 2020


TOKYO--Toshiba Electronic Devices & Storage Corporation (“Toshiba”) and its manufacturing subsidiary, Japan Semiconductor Corporation, have developed technology to improve the reliability of P-channel Laterally Double Diffused MOS (Pch-LDMOS) technology for analog ICs. The companies clarified the cause of degradation of breakdown voltage that occurs in the drain avalanche hot-carrier (DAHC) stress test, a reliability test for LDMOS, and identified a device structure that suppresses the degradation.

Details were reported at the IEEE-sponsored International Symposium on Power Semiconductor Devices and ICs 2020 (ISPSD 2020) held online.

The electrification of vehicles and automation of industrial equipment is stimulating demand for analog ICs that can maintain high reliability over the long term in low- and high-temperature environments. This has drawn increasing interest in LDMOS, which has low on-resistance that makes it suitable for a wide range of application.

In the drain avalanche hot-carrier (DAHC) stress test, LDMOS reliability is evaluated by applying a medium voltage to its gate over a long period. The test measures degradation of breakdown voltage, a known cause of damage and reduced reliability in analog ICs.

Until now, the mechanism that causes the degradation in breakdown voltage was not clear, but widely assumed to be due to a trapped charge in the corner of the shallow trench isolation (STI) [1], where the impact-ionization rate is the highest. The two companies’ investigation of electron flow and device structure found that the cause was different, a trapped charge in the bottom STI, not the corner.

The companies found that the RESURF structure [2] is more tolerant of breakdown voltage degradation than the more commonly used DRIFT structure [3], because an additional junction underneath the drift region shares balances the total electric field across the region. The RESURF structure suppresses degradation to two-thirds that of the DRIFT structure. [4]

Cross sections of DRIFT and RESURF Pch-LDMOS structures

Cross sections of DRIFT and RESURF Pch-LDMOS structures

Improved reliability demonstrated by the DAHC stress test

Improved reliability demonstrated by the DAHC stress test

Notes:
[1] STI: Shallow Trench Isolation. This divides elements or electrodes by embedding insulator film into shallow trenches.
[2] Comparison of breakdown voltage degradation in DAHC stress test after 5.5 hours. Breakdown voltage in the DRIFT structure falls 7.6V, but in the RESURF structure, it falls only 2.8V.
[3] DRIFT structure: an LDMOS structure in which the P-channel drift region is surrounded by the same P-channel region.
[4] RESURF structure: an LDMOS structure in which the P-channel drift region is surrounded by the N-channel region.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

A new window will open