February 25, 2020
Toshiba Electronic Devices & Storage Corporation
- Launch of U-MOS X-H Series adopting Toshiba’s latest generation process -
TOKYO— Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has released “XK1R9F10QB,” a 100V N-channel power MOSFET suitable for automotive 48V equipment applications such as load switches, switching power supplies and driving of motors. Shipments start today.
The new product is the first in Toshiba’s new U-MOS X-H Series of MOSFET with a trench structure, and is fabricated with the company’s latest[1] generation process. Mounted on a low-resistance TO-220SM(W) package, it delivers industry-leading low On-resistance[2], with a maximum On-resistance of 1.92mΩ, an approximate 20% reduction against the current “TK160F10N1L.” This advance helps to reduce equipment power consumption. It also delivers reduced switching noise, due to optimization of capacitance characteristics, which helps to reduce EMI[3] of equipment. In addition, the threshold voltage width is tightened to 1V to enhance switching synchronization when used in parallel.
Automotive equipment (Load switches, switching power supplies and motor drives, etc.)
RDS(ON)=1.92mΩ (max) @VGS=10V
(@Ta=25°C)
Part Number |
Polarity |
Absolute maximum ratings |
Drain-source On-resistance RDS(ON) max (mΩ) |
Channel- to-case thermal impedance Zth(ch-c) max (℃/W) |
Package |
Series |
||||
|---|---|---|---|---|---|---|---|---|---|---|
Drain- source voltage VDSS (V) |
Drain current (DC) ID (A) |
Drain current (pulsed) IDP (A) |
Channel temperature Tch (℃) |
@VGS =6V |
@VGS =10V |
|||||
N-channel |
100 |
160 |
480 |
175 |
3.31 |
1.92 |
0.4 |
TO-220SM(W) |
U-MOS X-H |
|
Notes:
[1] As of February 25, 2020
[2] Comparison with products with the same VDSS maximum rating and package class; According to a Toshiba survey, as of February 25, 2020.
[3] EMI (Electro Magnetic Interference)
Follow the link below for more on the new product.
Follow the link below for more on Toshiba Automotive MOSFETs.
*Company names, product names, and service names may be trademarks of their respective companies.
Customer Inquiries:
Power Device Sales & Marketing Department
Tel: +81-3-3457-3933
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.