Toshiba Introduces 5 new groups of TXZ+™ Family Advanced Class Microcontrollers that Realize Low Power Consumption, Support System Cost Reduction and Motor Control

January 13, 2021

Toshiba Electronic Devices & Storage Corporation

- Based on Arm® Cortex®-M core with integrated large capacity flash memory

TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") introduces five groups of new microcontrollers, which belong to the TXZ+™ family. The M4K, M4M, M4G, and M4N groups are based on the Arm Cortex-M4 core, and the M3H group is based on the Arm Cortex-M3 core. All groups offer low power consumption, suitable for a wide variety of applications such as motor control, connected IoT devices, leading-edge sensing functionalities, etc.

Engineering samples will start to ship in the fourth quarter of FY2020 (January to March 2021) and mass production will start in the second quarter of FY2021 (July to September 2021). Associated documentation, development tools and sample software will also be provided.

The advanced class has a maximum operating frequency of 200MHz, flash memory of max. 2MB and 12-bit analog-to-digital converters. They are equipped with application-focused peripherals such as high-efficiency motor control engines or rich connectivity interfaces.

Key Features

<Arm Cortex-M4 core >

  • M4K Group
    Motor control hardware, self-diagnosis function for home appliance functional safety standard IEC 60730
  • M4M Group
    Motor control hardware, CAN interface, self-diagnosis function for home appliance functional safety standard IEC 60730
  • M4G Group
    Maximum operating frequency of 200MHz, flash memory of max. 2MB, interfaces for high- speed communications, analog circuits for multiple sensor connections, high reliability firmware updating for secure processing
  • M4N Group
    Maximum operating frequency of 200MHz, max. 2MB flash memory, various interfaces for IoT devices (sensing and communication), supporting high speed data transfers

<Arm Cortex-M3 core >

  • M3H Group
    Integrated LCD display function, self-diagnosis function for home appliance functional safety standard IEC 60730, high efficiency motor controls, system cost reduction by reducing BOM

To learn more about the Toshiba TXZ+ family advanced class, visit:

TXZ+™ Family Advanced Class - New Products

* Arm and Cortex are registered trademarks of Arm limited (or its subsidiaries) in the US and/or elsewhere.
* TXZ+™ is a trademark of Toshiba Electronic Devices & Storage Corporation.
* Other company names, product names, and service names may be trademarks of their respective companies.

 

Customer Inquiries

System Devices Marketing Dept.II
Multi Marketing Group II

Tel: +81-3-3457-3465

* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.