March 11, 2021
Toshiba Electronic Devices & Storage Corporation
TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched 650V super junction power MOSFETs, TK065U65Z, TK090U65Z, TK110U65Z, TK155U65Z and TK190U65Z, in its DTMOSVI series that are housed in a TOLL (TO-leadless) package. Volume production shipments start today.
TOLL is a surface-mount package that has an approximately 27% smaller footprint than the usual D2PAK package. It is also a 4-pin type package that allows Kelvin connection of its signal source terminal for the gate drive. This can reduce the influence by the inductance of the source wire in the package to bring out the high-speed switching performance of the MOSFETs, suppressing oscillation when switching. Compared to Toshiba’s current product, TK090N65Z[1], the turn-on switching loss is reduced by about 68% and turn-off switching loss by about 56%[2][3]. The new MOSFETs are suitable for power supplies for industrial equipment such as data centers and photovoltaic power conditioners.
The combination of TOLL packaging with the latest[4] generation DTMOSVI process technology extends the line-up to cover a low On-resistance of up to 65mΩ(max)[5]. Toshiba will continue to enhance products with the TOLL package to contribute to equipment downsizing and improved efficiency.
Notes:
[1] A product in DTMOSVI series with equivalent voltage and On-resistance that uses the TO-247 package without Kelvin connection
[2] As of March 10, 2021, values measured by Toshiba (Test condition: VDD=400V, VGG=+10V/0V, ID=15A, Rg=10Ω, Ta=25℃).
[3] TK090U65Z only
[4] As of March 10, 2021
[5] TK065U65Z only
(Ta=25°C)
Part number |
||||||
|---|---|---|---|---|---|---|
Package |
Name |
TOLL |
||||
Size typ. (mm) |
9.9x11.68, t:2.3 |
|||||
Absolute maximum ratings |
Drain- source voltage VDSS (V) |
650 |
||||
Drain current (DC) ID (A) |
38 |
30 |
24 |
18 |
15 |
|
Drain-source On-resistance RDS(ON) max (Ω) @VGS=10V |
0.065 |
0.09 |
0.11 |
0.155 |
0.19 |
|
Total gate charge Qg typ. (nC) |
62 |
47 |
40 |
29 |
25 |
|
Gate-drain charge Qgd typ. (nC) |
17 |
12 |
11 |
8 |
7.1 |
|
Input capacitance Ciss typ. (pF) |
3650 |
2780 |
2250 |
1635 |
1370 |
|
Channel-to-case thermal resistance Rth(ch-c) max (℃/W) |
0.462 |
0.543 |
0.657 |
0.833 |
0.961 |
|
Conventional series (DTMOSIV) Part number |
- |
- |
- |
TK20G60W[6] |
TK16G60W[6] |
|
Sample Check & Availability |
||||||
Note:
[6] VDSS=600V, D2PAK package
Customer Inquiries:
Power Device Sales & Marketing Department
Tel: +81-3-3457-3933
*Company names, product names, and service names may be trademarks of their respective companies.
*Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.