November 18, 2021
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched a high voltage transistor output automotive photocoupler, “TLX9188,” for isolated signal communication in automotive equipment, including electric mobility vehicles. Volume shipments start today.
TLX9188’s high voltage photo transistor delivers a collector-emitter voltage rating of 200V, 2.5 times higher than Toshiba’s current TLX9185A, a first for the company[1]. By specifying maximum values for switching characteristics (turn-on time, turn-off time), the new photocoupler can be used as a unidirectional switch. It can also be used in feedback circuits of analog signals in 100V to 200V equipment, helping to reduce the cost of application circuits.
Note:
[1] For an automotive photocoupler
Automotive equipment
(Unless otherwise specified, @Ta=25°C)
Part number |
|||
|---|---|---|---|
Absolute maximum ratings |
Input forward current IF (mA) |
30 |
|
Collector current IC (mA) |
50 |
||
Operating temperature Topr (°C) |
-40 to 125 |
||
Electrical characteristics |
Collector-emitter breakdown Voltage V(BR)CEO min (V) |
@IC=0.1mA, Ta= -40 to 125°C |
200 |
Dark current ICEO max (μA) |
@VCE=200V |
0.2 |
|
Coupled electrical characteristics |
Current transfer ratio IC/IF min (%) |
@IF=5mA, VCE=5V, rank GB |
100 |
Saturated current transfer ratio IC/IF(sat) min (%) |
@IF=1mA, VCE=0.4V, rank GB |
30 |
|
Collector-emitter saturation voltage VCE(sat) max (V) |
@IC=2.4mA, IF=8mA |
0.4 |
|
OFF-state collector current IC(off) max (μA) |
@VF=0.7V, VCE=200V |
10 |
|
Switching characteristics |
Turn-on time tON max (μs) |
@RL=1.9kΩ, VCC=5V, IF=10mA |
100 |
Turn-off time tOFF max (μs) |
500 |
||
Isolation characteristics |
Isolation voltage BVS min (Vrms) |
3750 |
|
Package |
Name |
4pin SO6 |
|
Size typ. (mm) |
3.7×7.0×2.1 |
||
Sample Check & Availability |
|||
Follow the link below for more on the new product.
TLX9188
Follow the link below for more on Toshiba’s photocouplers.
Isolators/Solid State Relays
Follow the link below for more on Toshiba’s automotive devices.
Automotive Devices
To check availability of the new product at online distributors, please visit:
TLX9188

Customer Inquiries
Optoelectronic Device Sales & Marketing Dept.
Tel: +81-44-548-2218
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.