3글자 이상 입력하세요.
About information presented in this cross reference
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
June 7, 2022
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan—Toshiba Electronic Devices & Storage Corporation ("Toshiba") has added five products to its lineup of MOSFET gate driver ICs in the TCK42xG Series for mobile devices such as wearables. The new products in the series are equipped with an overvoltage lockout function and control the gate voltage of an external MOSFET according to the input voltage.
The new products are: “TCK420G” for 24V power lines; “TCK422G” and “TCK423G” for 12V power lines; “TCK424G” for 9V power lines; and “TCK425G” for 5V power lines. Along with the already launched “TCK421G” for 20V power lines, they are available now.
With this addition, TCK42xG series now allow users to select a gate-source voltage from two types, 10V and 5.6V, offering coverage of more MOSFETs. In addition, the lineup of the different detection voltages for the input overvoltage lockout function allows the products to be used for power lines from 5V to 24V. When combined with an external back-to-back MOSFET, they are also suitable for configuring a load switch circuit (Fig.1) or a power multiplexer circuit (Fig.2). with a reverse current blocking function. Furthermore, with their built-in charge pump circuit supporting a wide range of input voltages, from 2.7V to 28V, they provide stable voltage between the gate and source of an external back-to-back MOSFET with intermittent operation. This allows large currents to be switched.
Housed in a WCSP6G[1] package, one of the smallest in the industry[2], the TCK42xG series realizes high density mounting for small devices, such as wearables and smartphones, helping to reduce their footprint.
Toshiba has also developed “Power multiplexer circuit” Reference Design, a reference design example for a power multiplexer that utilizes the functions of TCK42xG. It is available on Toshiba’s website from today.
Notes :
[1] A 1.2mm × 0.8mm chip scale package
[2] Among MOSFET gate driver ICs, Toshiba survey as of June 2022.
(Unless otherwise specified, Ta=25°C)
Note:
[3] Already released product
Customer Inquiries
Small Signal Device Sales & Marketing Dept.
Tel: +81-44-548-2215
* Company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.