This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Two N-channel MOSFETs are externally connected back-to-back (in a common-source configuration or a common-drain configuration) when a load switch using a gate drive IC needs a function for blocking the current flowing into the load switch in the reverse direction. This function is called reverse-current blocking.
Power multiplexer circuit with 2 input and 1 output is implemented on a small PCB.
Please visit and download below for more detail
Please also refer to the following documents for related explanations.
Application note
FAQ
To product list of load switch ICs :
Main web page about load switch ICs
Other information