January 31, 2023
Toshiba Electronic Devices & Storage Corporation
KAWASAKI, Japan — Toshiba Electronic Devices & Storage Corporation ("Toshiba") has launched automotive 40V N-channel power MOSFETs, “XPQR3004PB” and “XPQ1R004PB,” that use the new L-TOGL™ (Large Transistor Outline Gull-wing Leads) package and feature a high drain current rating with low On-resistance. Shipments start today.
In recent years, the transition to EVs has fueled demand for components adapted to the increased power consumption of automotive equipment. The new products use Toshiba’s new L-TOGL™ package, which supports large currents, low resistance, and high heat dissipation. The products do not have an internal post[1] structure, achieved by unifying the source connective part and outer leads with a copper clip. A multi-pin structure for the source leads decreases package resistance to about 30% that of the existing TO-220SM(W) package, pushing the drain current (DC) rating of XPQR3004PB to 400A—1.6 times higher than that of the current product[2]. Use of a thick copper frame has cut channel-to-case thermal impedance in XPQR3004PB to 50% that of the current product[2]. These features help larger current and lower the loss of automotive equipment.
With the new package technology, the new products will simplify heat dissipation design and lower the number of MOSFETs required in applications such as semiconductor relays and invertors for integrated starter generators that require large currents, and help to reduce equipment size. Assuming that multiple devices will be connected in parallel for applications requiring higher-current operation, Toshiba supports grouping shipment[3] for the new products, in which the gate threshold voltage is used for grouping. This allows designs using product groups with small characteristic variation.
Since automotive equipment is used in diverse temperature environments, the reliability of solder joints in surface mounting is a critical consideration. The new products use gull-wing leads that reduce mounting stress, improving the reliability of the solder joint.
Notes:
[1] Solder connection
[2] Current product: “TKR74F04PB” with TO-220SM(W) package
[3] Toshiba can offer grouping shipment in which the gate threshold voltage range is 0.4V for each reel. However, specifying a specific group is not possible. Please contact Toshiba sales representatives for more details.
(Ta=25°C unless otherwise specified)
| Part number | Polarity | Absolute maximum ratings | Drain-source On-resistance RDS(ON) max (mΩ) |
Channel-to-case thermal impedance Zth(ch-c) max at Tc=25°C (℃/W) |
Package | Series | Sample Check & Availability | ||||
|---|---|---|---|---|---|---|---|---|---|---|---|
Drain- source voltage VDSS (V) |
Drain current (DC) ID (A) |
Drain current (pulsed) IDP (A) |
Channel temperature Tch (°C) |
at VGS=6V |
at VGS=10V |
||||||
| XPQR3004PB | N-channel |
40 |
400 |
1200 |
175 |
0.47 |
0.30 |
0.2 |
L-TOGL™ |
U-MOSIX-H |
![]() |
| XPQ1R004PB | N-channel |
40 |
200 |
600 |
175 |
1.8 |
1.0 |
0.65 |
L-TOGL™ |
U-MOSIX-H |
![]() |
Follow the links below for more on the new products.
XPQR3004PB
XPQ1R004PB
Follow the links below for more on the related content on the new products.
Follow the link below for more on Toshiba Automotive MOSFETs.
Automotive MOSFETs
To check availability of the new products at online distributors, visit:
XPQR3004PB

Customer Inquiries:
Power Device Sales & Marketing Department
Tel: +81-44-548-2216
* L-TOGL™ is a trademark of Toshiba Electronic Devices & Storage Corporation.
* Other company names, product names, and service names may be trademarks of their respective companies.
* Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.