December 7, 2016
Suited to Digital Home Appliances, Industrial Equipment
IRVINE, Calif., --- Toshiba America Electronic Components, Inc. (TAEC)* today announced the availability of a line of CMOS logic ICs in small outline integrated circuit (SOIC) packages: the 74HCxxxD series. These products support flow and reflow soldering, and are suitable for industrial equipment and digital home appliances with logic levels of 6V and lower. The 63 new part numbers in the 74HCxxxD series consist of the most commonly used 74-series logic functions, bringing the total number of CMOS logic ICs offered by Toshiba to more than 300.
An SOIC is a surface-mounted integrated circuit that occupies an area that is approximately 30–50 percent less than an equivalent dual in-line package (DIP) with a thickness that is 70 percent smaller. This smaller size is well suited to applications that require a smaller PCB footprint. Toshiba’s ICs are available in industry standard packages of SOIC14, SOIC16, and SOIC20, and include a range of functionalities such as various gate types, flip flops, buffers, multiplexers, serial/parallel shift registers and more.
Part Number |
Logic Function |
---|---|
74HC00D |
Quad 2-input NAND gate |
74HC02D |
Quad 2-input NOR gate |
74HC03D |
Quad 2-input NAND gate with open-drain |
74HC08D |
Quad 2-input AND gate |
74HC21D |
Dual 4-input NAND gate |
74HC32D |
Quad 2-input OR gate |
74HC86D |
Quad 2-input XOR gate |
74HC04D |
Hex inverter |
74HC05D |
Hex inverter with open-drain |
74HC14D |
Hex schmitt inverter |
74HC123D |
Dual monostable multivibrator |
74HC125D |
Quad 3-state buffer |
74HC132D |
Quad 2-input Schmitt NAND |
74HC138D |
3-to-8 line Demultiplexor |
74HC139D |
Dual 2-to-4 Demultiplexor |
74HC151D |
8-to-1 Multiplexor |
74HC153D |
Dual 4-to-1 Multiplexor |
74HC157D |
Quad 2-to-1 Multiplexor |
74HC164D |
Parallel-out 8-bit Shift Register |
74HC166D |
Parallel-in 8-bit Shift Register |
74HC74D |
Dual D Flip-Flop |
74HC174D |
Hex D Flip-Flop |
74HC175D |
Quad D Flip-Flop |
74HC244D |
Octal buffer with 3-state outputs |
74HC245D |
Octal bus transceiver with 3-state outputs |
74HC259D |
8-bit addressable latch |
74HC273D |
8-bit register with asynchronous clear |
74HC373D |
Octal transparent latch with 3-state outputs |
74HC374D |
Octal register with 3-state outputs |
74HC393D |
Dual 4-bit binary counter |
74HC540D |
Inverting octal buffer with 3-state outputs |
74HC541D |
Non-inverting octal buffer with 3-state outputs |
74HC573D |
Octal D-type transparent latch with 3-state outputs |
74HC4049D |
Hex inverting Buffer |
74HC4050D |
Hex non-inverting Buffer |
74HC4051D |
8-channel analog Mux/Demultiplexer |
74HC4052D |
Dual 4-channel analog Mux/Demultiplexers |
74HC4053D |
Triple 2-channel analog Mux/Demultiplexers |
74HC4066D |
Quad Bilateral Switches |
Toshiba’s new CMOS logic ICs in SOIC packages are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide (as of March 31, 2016). Visit Toshiba's web site at http://toshiba.semicon-storage.com.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.