Toshiba Announces Compact Intelligent Power device with 600V Rating

May 28, 2020

Efficient operation reduces power consumption of motor equipment

Toshiba TPD4162F

Toshiba America Electronic Components, Inc.  (“Toshiba”) has announced a high voltage intelligent power device intended for driving the motor within equipment such as air conditioners, air cleaners and pumps. With its rated power supply voltage (VBB) of 600V, the TPD4162F can be used for any applications with input signals in the range 200 to 220VAC.

The new IC contains a PWM circuit, 3-phase decoder, level shifting high-side driver and low side driver with embedded IGBTs and FRDs. This allows direct drive of brushless DC (BLDC) motors with square wave input signals from a Hall sensor or Hall IC without the requirement for a PWM controller IC. 

Based upon a new process, the TPD4162F offers reduced power dissipation of approximately 10% compared its predecessor (TPD4152F), reducing the power dissipation of motor drivers. 

Multiple protection features including current limit, over current protection (OCP), thermal shutdown and undervoltage lockout (UVLO) are built in thereby reducing the need for peripheral circuits. This, along with the small HSSOP31 surface mount package with a 17.5 x 11.9mm footprint and 2.2mm height, allows for compact designs including the ability to mount the driver circuitry directly to the motor.  

Mass production has started and the first shipments will be made today.

Follow the link below for more on the new product.

TPD4162F

About Toshiba America Electronic Components, Inc.

Toshiba America Electronic Components, Inc. (TAEC), an independent operating company owned by Toshiba America, Inc., is the US based electronic components business of Toshiba Electronic Devices and Storage Corporation. TAEC offers a wide variety of innovative hard disk drive (HDD) products and semiconductor solutions for data center, automotive, industrial, IoT, motion control, telecom, networking, consumer, and white goods applications. The company’s broad portfolio encompasses enterprise and consumer HDDs integrated wireless ICs, power semiconductors, microcontrollers, optical semiconductors.


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

A new window will open