September 30, 2019
Toshiba Electronic Devices & Storage Corporation
 
            
        
    TOKYO—Toshiba Electronic Devices & Storage Corporation ("Toshiba") today announced the launch of “TB67B000AHG,” a new three-phase brushless motor driver for home appliances such as air-conditioners, air-purifiers, dehumidifiers, and ceiling fans. The new driver is a high-voltage addition to the “TB67B000 series,” which realizes highly efficient brushless motor drive and noise reduction in a single package.
Demand is growing, particularly in emerging economies, for high-efficiency three-phase brushless fan motors that can reduce energy consumption and can manage fluctuations in power voltage. Such motors require higher-voltage PWM driver ICs to maintain high product reliability.
Toshiba’s newly developed 600V TB67B000AHG driver IC is pin-compatible with the current 500V TB67B000HG and can easily replace it. Toshiba is also developing the more compact version “TB67B000AFG” in a small 34-pin HSSOP [1] package which will be available in November 2019.
Home appliances such as air-conditioners and air-purifiers, dehumidifiers, ceiling fans, and other industrial equipment.
[1]: Shrink Small Outline Package with Heat Sink
* Company names, product names, and service names may be trademarks of their respective companies.
Customer Inquiries
System Devices Marketing Dept.II
Tel: +81-3-3457-3332
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.