January 20, 2020
Toshiba Electronic Devices & Storage Corporation
- Supports IEC 61131-2 digital input type 1 -
TOKYO—Toshiba Electronic Devices & Storage Corporation (“Toshiba”) has launched “TLP2363,” a 10Mbps high-speed communication logic output photocoupler for 24V digital input interfaces of Programmable Logic Controllers (PLCs). Shipments start today.
The new photocoupler’s specifications include both the minimum and maximum values of its threshold input current at its operating temperature range (-40 to 105℃). Use of the photocoupler in combination with appropriate resistors for current control realizes a 24V digital input module that follows IEC 61131-2 Type 1[1] specifications.
In addition, the new product’s circuit suppresses chattering noise so that its output is clearly either “low” or “high,” even with a slow input signal with a long (60s or less) rise or fall time. This eliminates the need for a waveform shaping circuit in the output part, reducing the number of components.
The photocoupler is packaged in the thin 5pin SO6, and has a maximum height of 2.3mm. Its slim shape brings greater freedom to component layout on printed circuit boards.
(Unless otherwise specified, @Ta= -40 to 105℃)
Note:
[1] Specifies the requirements and tests for PLC devices
Follow the link below for more on the new product.
Follow the link below for more on Toshiba’s optical devices line-up.
* Company names, product names, and service names may be trademarks of their respective companies.
Customer Inquiries
Optoelectronic Device Sales & Marketing Dept.
Tel: +81-3-3457-3431
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.