Toshiba Introduces New 20V MOSFETs with Low On-Resistance Specifications

 July 27, 2017

Toshiba SOT-23F packages

IRVINE, Calif., --- Toshiba America Electronic Components, Inc. (TAEC)* has introduced four new 20V MOSFETs that feature some of the lowest on-resistance specifications in the industry. Housed in small SOT-23F packages, the SSM3K344R, SSM3K345R, SSM3J355R and SSM3J358R are suitable for lowering the power consumption in power supply controls for individual function blocks, or for power supply distribution. Applications include mobile devices, such as PCs, laptops and tablets, in addition to other consumer products and industrial equipment.

Toshiba’s lineup of SOT-23F package MOSFETs provide a simple FET switch functionality for power rails up to 40V, at currents up to 6A. The company’s UMOSVII-H MOSFET process allows for a significant reduction in gate switch charge and on-state resistance (RDS(ON)) when compared to the previous MOSFET process, resulting in greater power efficiency. Toshiba’s SOT-23F package (2.4x2.9mm) offers superior power dissipation and can be installed in the industry-standard SOT-23 package land pattern.

The new 20V products achieve low on-resistance by utilizing the latest low voltage trench structure process and feature a highly allowable power dissipation rating (2.4x2.9mm, PD=1.0 W1).

Main Specifications 

(@Ta=25°C)

Part number Package Polarity Absolute maximum ratings Electrical characteristics
Drain-source voltage VDSS (V)

Gate-source voltage VGSS (V)

Drain current ID (A)

Power dissipation PD1(W)

Drain-source 
On-resistanceRDS(ON) typ.(
mΩ)
Input capacitance Ciss typ.  (pF)

@|VGS|

=4.5V

@|VGS|

=1.8V

SSM3K344R

 SOT-23F

N-ch

20

±8

3

1

51.0

81.0

153

SSM3K345R

N-ch

20

±8

4

1

25.0

40.0

410

SSM3J355R

P-ch

-20

±10

-6

1

23.0

36.0

1030

SSM3J358R

P-ch

-20

±10

-6

1

19.3

28.8

1331

Pricing and Availability

The SSM3K344R, SSM3K345R, SSM3J355R and SSM3J358R are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.

*About TAEC

Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide.  A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), solid state hybrid drives (SSHDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, and advanced materials that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more.

Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan’s largest semiconductor, solid state drive and hard disk drive manufacturer and the world’s seventh largest semiconductor manufacturer (Gartner, 2015 Worldwide Semiconductor Revenue, January, 2016). Founded in Tokyo in 1875, Toshiba is at the heart of a global network of over 550 consolidated companies employing over 188,000 people worldwide (as of March 31, 2016). Visit Toshiba's web site at http://toshiba.semicon-storage.com.

1 Device mounted on a 25.4×25.4×1.6mm FR-4 glass epoxy board (Cu pad: 645mm2)


Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.

A new window will open