August 16, 2017
Targeted to Mobile Applications; Capable of Driving up to 420mA
IRVINE, Calif., --- Toshiba America Electronic Components, Inc. (TAEC)* today announced a new family of CMOS low dropout (LDO) regulators: the TCR4DG series. Consisting of general-purpose, single-output voltage regulators with on/off control input, low output noise voltage and low inrush current, the TCR4DG series is available in fixed output voltages between 1.0V and 4.5V – capable of driving up to 420mA.
Small ceramic input and output capacitors can be used with the TCR4DG series, making these devices suitable for mobile applications that require high-density board assembly, such as cell phones. The new regulators are offered in an ultra-small plastic mold WCSP4E package (0.645mmx0.645mm (typical); t:0.43mm (max)) and feature over-current protection, over-temperature protection, inrush current protection, and auto-discharge functionality.
“Mobile designs are becoming increasingly power hungry and are demanding high-current LDOs to fit inside compact designs,” noted Talayeh Saderi, senior business development manager for TAEC. “With the new TCR4DG series, we’re providing engineers with 400mA of clean, efficient voltage regulation in a small package – the 420mA LDO.”
Product No. |
Output voltage |
Marking |
Product No. |
Output voltage (V)(typ.) |
Marking |
|---|---|---|---|---|---|
TCR4DG10 |
1.0 |
A |
TCR4DG25 |
2.5 |
T |
TCR4DG105 |
1.05 |
B |
TCR4DG27 |
2.7 |
U |
TCR4DG11 |
1.1 |
C |
TCR4DG275 |
2.75 |
V |
TCR4DG115 |
1.15 |
D |
TCR4DG28 |
2.8 |
W |
TCR4DG12 |
1.2 |
E |
TCR4DG285 |
2.85 |
X |
TCR4DG125 |
1.25 |
F |
TCR4DG29 |
2.9 |
Y |
TCR4DG13 |
1.3 |
H |
TCR4DG30 |
3.0 |
0 |
TCR4DG135 |
1.35 |
J |
TCR4DG31 |
3.1 |
1 |
TCR4DG15 |
1.5 |
K |
TCR4DG32 |
3.2 |
2 |
TCR4DG175 |
1.75 |
L |
TCR4DG325 |
3.25 |
3 |
TCR4DG18 |
1.8 |
M |
TCR4DG33 |
3.3 |
4 |
TCR4DG185 |
1.85 |
N |
TCR4DG35 |
3.5 |
5 |
TCR4DG19 |
1.9 |
P |
TCR4DG36 |
3.6 |
6 |
TCR4DG23 |
2.3 |
R |
TCR4DG42 |
4.2 |
7 |
TCR4DG245 |
2.45 |
S |
TCR4DG45 |
4.5 |
8 |
Toshiba’s new CMOS LDO voltage regulators are available now. For more details, samples and pricing information, please contact your local Toshiba Sales Office.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, solid state drives (SSDs), hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, advanced materials and medical tubes that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions and more .
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba promotes global operations that contribute to realization of a world where generations to come can live better lives.
To find out more about Toshiba, visit www.toshiba.co.jp/worldwide/about/index.html.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications.