November 27, 2017
The MD06ACA-V Series is Toshiba’s largest capacity surveillance-class HDD
IRVINE, Calif. — Toshiba America Electronic Components, Inc., a committed technology leader, announces the MD06ACA-V, the latest addition to its SV Series line-up of 3.5-inch hard drives for surveillance applications. The new models are available in capacities up to 10TB1 with higher transfer rate compare with previous generations, and can support up to 64 cameras2 operating 24/7. These key benefits are the ability to support higher resolution camera streams.
The MD06ACA-V Series is designed for streaming operation scenarios, and typically used for surveillance digital video recorders (SDVR), surveillance network video recorders (SNVR) and Hybrid SDVR. Compared to previous generations, it features a 7,200 rpm higher access performance, and a 58 percent increase in the maximum sustained transfer rate, pushing it to 237MiB/s3. Available in 6TB, 8TB and 10TB capacities, the new drive models provide a SATA 6Gbit/s interface4, with a 256MiB dynamic buffer. Additionally, the MD06ACA-V models support Advanced Format (512e) technology for compatibility with legacy applications and operating environments.
“Our third generation surveillance HDD line-up provides the capacity, performance and reliability needed for today’s higher resolution surveillance video streams and longer content retention requirements,” said Scott Wright, Director of HDD Product Marketing at Toshiba America Electronic Components, Inc. “The new Toshiba models include RV compensation technology for optimal performance in multi-bay configurations, and provide excellent reliability with a mean time to failure (MTTF)5 of 1 million hours utilizing a conventional mechanical design.”
Samples of the MD06ACA-V Series are now available. For more information on the full line of Toshiba HDD products, please visit: http://toshiba.semicon-storage.com/us/product/storage-products.html. To learn more about Toshiba storage solutions visit the storage blog at http://storage.toshiba.com/corporateblog/ and follow @ToshibaStorage on Twitter.
About Toshiba Group. and Toshiba America Electronic Components, Inc.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba Group enables its customers to create market-leading designs. Toshiba Group is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba Group designs and manufactures high-quality hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, and advanced materials that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions, consumer products and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation and its affiliates/subsidiaries has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba Group promotes global operations that contribute to realization of a world where generations to come can live better lives. Visit our web site at http://toshiba.semicon-storage.com.
1We define a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
2Number of surveillance cameras support capability is defined by performance simulation with High Definition cameras at 10Mbit/s rate. Actual results may vary based on various factors, including the types of cameras installed, the system’s hardware and software capabilities, and the video compression technology used, as well as system variables such as resolution, frames per second, and other settings.
3A mebibyte (MiB) means 220, or 1,048,576 bytes.
4Read and write speed may vary depending on the host device, read and write conditions, and file size.
5MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba Group enables its customers to create market-leading designs. Toshiba Group is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, VARs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba Group designs and manufactures high-quality hard disk drives (HDDs), discrete devices, custom SoCs/ASICs, imaging products, microcontrollers, wireless components, mobile peripheral devices, and advanced materials that make possible today’s leading smartphones, tablets, cameras, medical devices, automotive electronics, industrial applications, enterprise solutions, consumer products and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc. For over 140 years, Toshiba Corporation and its affiliates/subsidiaries has contributed to a sustainable future by applying innovative technologies to value creation. Today, our business domains are centered on the essential infrastructure that supports modern life and society. Guided by the principles of The Basic Commitment of the Toshiba Group, “Committed to People, Committed to the Future”, Toshiba Group promotes global operations that contribute to realization of a world where generations to come can live better lives. Visit our web site at http://toshiba.semicon-storage.com.
1We define a megabyte (MB) as 1,000,000 bytes, a gigabyte (GB) as 1,000,000,000 bytes and a terabyte (TB) as 1,000,000,000,000 bytes. A computer operating system, however, reports storage capacity using powers of 2 for the definition of 1GB = 230 = 1,073,741,824 bytes and therefore shows less storage capacity. Available storage capacity (including examples of various media files) will vary based on file size, formatting, settings, software and operating system and/or pre-installed software applications, or media content. Actual formatted capacity may vary.
2Number of surveillance cameras support capability is defined by performance simulation with High Definition cameras at 10Mbit/s rate. Actual results may vary based on various factors, including the types of cameras installed, the system’s hardware and software capabilities, and the video compression technology used, as well as system variables such as resolution, frames per second, and other settings.
3A mebibyte (MiB) means 220, or 1,048,576 bytes.
4Read and write speed may vary depending on the host device, read and write conditions, and file size.
5MTTF (Mean Time to Failure) is not a guarantee or estimate of product life; it is a statistical value related to mean failure rates for a large number of products which may not accurately reflect actual operation. Actual operating life of the product may be different from the MTTF.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Company names, product names, and service names mentioned herein may be trademarks of their respective companies.