March 20, 2019
IRVINE, Calif. – Toshiba America Electronic Components, Inc.(“Toshiba”) today announced two new series of small surface mount LDO regulators for application in the power supply of mobile devices, imaging and audio-visual products. The 40 regulators in the TCR5BM series support a dropout voltage as low as 100mV and a maximum output current of 500mA, and 40 more in the TCR8BM series extend support to 170mV and 800mA. The TCR5BM and TCR8BM series are both available with VOUT as low as 0.8V, or as high as 3.6V.
Both series are suited to applications that include power supply for MCU, RF devices, and camera CMOS sensors in mobile devices or imaging and audio-visual equipment, which increasingly use lower voltages around 1V.
Mass production started progressively from January 2019 and shipments begin today.
By using a low on-resistance N-channel MOSFET fabricated with the latest generation process and external bias voltage, both series have cut dropout voltage, a cause of power loss, to about 67% that of Toshiba’s current products1, the lowest in the industry2.
In addition, with a 98 dB (typ.) ripple rejection ratio, the new products deliver stable operation resistant to high frequency noise from the external environment and DC-DC converters, both causes of malfunction. They also deliver a fast load transient response that prevents malfunctioning due to swift switching of IC operation modes.
Quiescent current is about 50% lower than other high current LDO regulators in the market2, realizing lower power consumption by devices and longer operating times for battery-driven devices.
Both series are housed in the small surface mount 1.2x1.2mm DFN5B3 package, which is excellent for space constrained designs. The TCR5BM series supports up to 500mA and the TCR8BM series supports up to 800mA, allowing users to design products more easily.
Mobile devices, image & audio visual equipment
| Part Number | Package | Output voltage lineup | Electrical characteristics (@Tj=25 ℃) | ||||
|---|---|---|---|---|---|---|---|
| Name | Size typ. (mm) | Quiescent current IBIAS(ON) typ.(μA) | Dropout voltage VDO typ. | Ripple rejection ratio R.R. typ. (dB) |
|||
| (mV) | @IOUT (mA) |
||||||
TCR5BM series |
DFN5B |
1.2x1.2 |
0.8 to 3.6 V and 36 voltage |
19 |
100 |
500 |
98 |
TCR8BM series |
0.8 to 3.6 V and 36 voltage |
20 |
170 |
800 |
98 |
||
Stock Check & Purchase |
TCR5BM series Buy Online TCR8BM series Buy Online |
||||||
| No. | Output voltage VOUT typ. (V) |
Part number | No. | Output voltage VOUT typ. (V) |
Part number | ||
|---|---|---|---|---|---|---|---|
| TCR5BM series | TCR8BM series | TCR5BM series | TCR8BM series | ||||
1 |
0.8 |
TCR5BM08A* |
TCR8BM08A* |
21 |
1.9 |
TCR5BM19A* |
TCR8BM19A* |
2 |
0.85 |
TCR5BM085A* |
TCR8BM085A* |
22 |
2.0 |
TCR5BM20A* |
TCR8BM20A* |
3 |
0.9 |
TCR5BM09A* |
TCR8BM09A* |
23 |
2.1 |
TCR5BM21A* |
TCR8BM21A* |
4 |
0.95 |
TCR5BM095A* |
TCR8BM095A* |
24 |
2.2 |
TCR5BM22A* |
TCR8BM22A* |
5 |
1.0 |
TCR5BM10 |
TCR8BM10 |
25 |
2.3 |
TCR5BM23A* |
TCR8BM23A* |
6 |
1.0 |
TCR5BM10A* |
TCR8BM10A* |
26 |
2.4 |
TCR5BM24A* |
TCR8BM24A* |
7 |
1.05 |
TCR5BM105 |
TCR8BM105 |
27 |
2.5 |
TCR5BM25A* |
TCR8BM25A* |
8 |
1.05 |
TCR5BM105A* |
TCR8BM105A* |
28 |
2.6 |
TCR5BM26A* |
TCR8BM26A* |
9 |
1.1 |
TCR5BM11 |
TCR8BM11 |
29 |
2.7 |
TCR5BM27A* |
TCR8BM27A* |
10 |
1.1 |
TCR5BM11A* |
TCR8BM11A* |
30 |
2.8 |
TCR5BM28A* |
TCR8BM28A* |
11 |
1.15 |
TCR5BM115A* |
TCR8BM115A* |
31 |
2.85 |
TCR5BM285A* |
TCR8BM285A* |
12 |
1.2 |
TCR5BM12 |
TCR8BM12 |
32 |
2.9 |
TCR5BM29A* |
TCR8BM29A* |
13 |
1.2 |
TCR5BM12A* |
TCR8BM12A* |
33 |
2.95 |
TCR5BM295A* |
TCR8BM295A* |
14 |
1.25 |
TCR5BM125A* |
TCR8BM125A* |
34 |
3.0 |
TCR5BM30A* |
TCR8BM30A* |
15 |
1.3 |
TCR5BM13A* |
TCR8BM13A* |
35 |
3.1 |
TCR5BM31A* |
TCR8BM31A* |
16 |
1.4 |
TCR5BM14A* |
TCR8BM14A* |
36 |
3.2 |
TCR5BM32A* |
TCR8BM32A* |
17 |
1.5 |
TCR5BM15A* |
TCR8BM15A* |
37 |
3.3 |
TCR5BM33A* |
TCR8BM33A* |
18 |
1.6 |
TCR5BM16A* |
TCR8BM16A* |
38 |
3.4 |
TCR5BM34A* |
TCR8BM34A* |
19 |
1.7 |
TCR5BM17A* |
TCR8BM17A* |
39 |
3.5 |
TCR5BM35A* |
TCR8BM35A* |
20 |
1.8 |
TCR5BM18A* |
TCR8BM18A* |
40 |
3.6 |
TCR5BM36A* |
TCR8BM36A* |
Part numbers marked with an asterisk have a built-in under-voltage lockout function.
Toshiba America Electronic Components, Inc. (TAEC) an independent operating company owned by Toshiba America, Inc., is the US based electronic components business of Toshiba Electronic Devices and Storage Corporation. TAEC offers consumers and businesses a wide variety of innovative hard disk drive (HDD) products plus semiconductor solutions for automotive, industrial, IoT, motion control, telecoms, networking, consumer and white goods applications. The company’s broad portfolio encompasses integrated wireless ICs, power semiconductors, microcontrollers, optical semiconductors, ASICs, ASSPs and discrete devices ranging from diodes to logic ICs. For more company information visit TAEC’s web site at http://www.toshiba.semicon-storage.com/
1 In comparison with Toshiba’s current TCR5AM series.
2 Toshiba survey conducted March 20, 2019
3 DFN5B package: 1.2×1.2 mm (typ.)
Information in this document, including product prices and specifications, content of services and contact information, is current on the date of the announcement but is subject to change without prior notice.