This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
require 3 characters or more. Search for multiple part numbers fromhere.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
require 3 characters or more.
Toshiba Corporation has achieved an areal density of one terabit per square inch (1Tbit/ in2) within a 2.5-inch client hard disk drive (HDD). This newest disk drive innovation delivers 3TB capacity using a 750GB per platter in a 15mm 2.5-inch HDD and increases areal density over Toshiba’s prior generation of client HDDs by 40 percent. Toshiba is dedicated to developing new technologies to increase storage performance and capacities in consumer electronics. Toshiba’s high areal density HDDs will be available in new products shipping later this year.