This webpage doesn't work with Internet Explorer. Please use the latest version of Google Chrome, Microsoft Edge, Mozilla Firefox or Safari.
3글자 이상 입력하세요.
The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.
3글자 이상 입력하세요.
Instead of detecting the rotor position using sensors (Hall elements or a Hall IC), a sensorless motor drive system monitors changes in the motor back-EMF voltage to predict the timing of current conduction. However, applications in which the motor RPM fluctuates considerably because of load variations make it difficult to predict this timing accurately, causing the motor to fall out of step. (The motor stops rotating.)
If the back-EMF voltage is insufficient, it is difficult to realize stable sensorless drive. When the back-EMF voltage is low at low RPM, motor operation tends to become unstable.