White Papers

Mixing Hard Disk Drives of 512 Byte native and 512 Byte emulated Block Size in RAID Systems
Mixing Hard Disk Drives of 512 Byte native and 512 Byte emulated Block Size in RAID Systems (1.4MB)
Hard Disk Drives (HDDs) for NAS and Enterprise Storage come in two different flavors of block size. Traditionally, the internal block size of HDDs is 512 byte, with 512 byte also used at the external interface. This technology is called 512 byte native, or 512n. Newer HDD models use an internal block size of 4k byte for higher storage efficiency, but still provide 512 byte at the external interface through a transparent emulation process. This technology is called 512 byte emulated (512e). Additionally drives with the 4k byte internal block format at the interface (4k byte native) are available, but these are rare and exclusively used in specific enterprise applications.
High-Reliability FC-MAMR Nearline HDD with a Capacity of 18 TB
High-Reliability FC-MAMR Nearline HDD with a Capacity of 18 TB (829KB)
As demand for nearline HDDs for data centers is growing, the requirements for data storage solutions for both cyber and physical spaces are diversifying, making it necessary to develop new innovative technologies for not only reading but also writing data. High-reliability technologies are attracting plenty of attention as a means to overcome the limit to the HDD recording density and thereby solve the information explosion problem.
WhitePaper_nearlineHDD_16TB_e
High capacity 16TB HDD CMR HDD with two-dimensional magnetic recording (TDMR) (3.50MB)
The growth and prevalence of cloud services has set the stage for the increasing dissemination of different types of storage services for different types of data storage needs.
WhitePaper_14TBnearlineHDD_e
World’s first 14TB nearline HDD with Conventional Magnetic Recording (3.62MB)
With the prevalence of IoT, big-data, cloud, and other IT services, the volume of data generated is increasing exponentially.
Reliability of Enterprise Hard Disk Drives
Reliability of Enterprise Hard Disk Drives (224KB)
This paper discusses the various factors that impact upon the reliability of Hard Disk Drives (HDD).
whitepaper_wipetechnology_e
Wipe technology HDD(1.6MB)
In April 2011 Toshiba announced Wipe2 technology (later mention) Toshiba’s unique set of enhanced features for TCG-Opal selfencrypting disk drive (SED) models.
idc
IDC White Paper (114KB)
Enterprise customers are faced with an unprecedented diversity of choice when selecting the storage components and infrastructure for their datacenters and cloud environments.
magne_vol8-1
Toshiba Hybrid Drive with Large Capacity and High-Speed Performance (638KB)―An HDD integrated with NAND flash memory―
The Magnetics Society of Japan's Journal "Magnetics Japan" Volume 8, No. 1
tribology
Flying Instability due to Organic Compounds in Hard Disk Drive
Advances in Tribology Volume 2012 (2012), Article ID 170189, 6 pages
  • The product technology,company name etc. are at the time of publication.
  • Before creating and producing designs and using, customers must also refer to and comply with the latest versions of all relevant information of this document and the instructions for the application that Product will be used with or for.

문의

문의

문의

자주 있는 문의

자주 있는 문의

구매

구매처
A new window will open