Part Number Search

Cross Reference Search

About information presented in this cross reference

The information presented in this cross reference is based on TOSHIBA's selection criteria and should be treated as a suggestion only. Please carefully review the latest versions of all relevant information on the TOSHIBA products, including without limitation data sheets and validate all operating parameters of the TOSHIBA products to ensure that the suggested TOSHIBA products are truly compatible with your design and application.
Please note that this cross reference is based on TOSHIBA's estimate of compatibility with other manufacturers' products, based on other manufacturers' published data, at the time the data was collected.
TOSHIBA is not responsible for any incorrect or incomplete information. Information is subject to change at any time without notice.

Keyword Search

Parametric Search

Stock Check & Purchase

News Center

This page is listing links of the press release and topics published by Toshiba Electronic Devices and Storage Corporation.
Information in the news and topics, including product prices and specifications, content of services and contact information, is current on the date of the news announcement, but is subject to change without prior notice. The news before March 31, 2017 is the news published by Toshiba Storage & Electronic Devices Solutions Company.

Release Year
Product Category

03-09-2020
Toshiba's Latest Enterprise Hard Disk Drives Qualified for Microchip Technology’s Adaptec® HBAs and RAID Adapters
02-27-2020
Toshiba Introduces Cutting-edge Generation SOI Process for RF Switches and Low-Noise Amplifier ICs for 5G Smartphones
02-20-2020
Toshiba Adds New Low Power Consumption Brushed DC Motor Driver IC
02-07-2020
Toshiba Launches Compact, Low Power, High Resolution Micro-stepping Motor Driver IC
01-28-2020
Toshiba Launches Compact High-Speed Communication Logic Output Photocoupler for Programmable Logic Controllers
01-27-2020
Toshiba Materials to Open Second Production Site for Silicon Nitride Substrates
01-15-2020
A lineup expansion of small MOSFETs for automotive equipment offering low power consumption with low On-resistance: SSM6J808R, SSM6K819R
12-10-2019
Toshiba Launches General-Purpose System Power IC with Multiple Outputs for Automotive Functional Safety
12-03-2019
Toshiba’s New Three-Phase Brushless Motor Control Pre-Driver IC Features Sensorless Control and Closed Loop Speed Control
12-02-2019
Toshiba Releases Surveillance 6TB HDDs for DVR and NVR Platforms
11-26-2019
Toyota Lexus UX and Lexus NX with Toshiba’s Image Recognition Processor Win Highest Score in Japan’s Assessment of Preventive Safety Performance
11-20-2019
Toshiba Releases its First eFuse, an Electronic Fuse that can be Repeatedly Used
10-29-2019
Toshiba’s New Three-Phase Brushless Motor Control Pre-Driver IC Features Intelligent Phase Control and Closed Loop Speed Control
10-17-2019
Toshiba Releases Low Capacitance TVS Diodes Suitable for ESD Protection for Thunderbolt 3 and other High Speed Signal Lines
10-01-2019
Toshiba Launches 600V Sine-Wave PWM Driver IC for Three-Phase Brushless Motors
09-26-2019
Toshiba Launches High-voltage Dual-channel Solenoid Driver IC
09-25-2019
Toshiba Launches Voltage Driven Photorelay in Industry’s Smallest Package with Reduced Input Power Dissipation
09-03-2019
Low capacitance TVS diodes for automotive applications offering fine protection performance while keeping signal quality at several Gbps : DF2S5M4FS, DF2S6M4FS
08-20-2019
A lineup expansion of TVS diodes for mobile devices by a product with an increased peak pulse current rating for improved surge protection performance: DF2B7BSL
07-10-2019
Toshiba expands lineup of SBD, which uses a compact package with high heat dissipation ability that allows easier thermal design, by 30 V/ 40 V products: CUHS20F40, CUHS20F30, CUHS15F40, CUHS15F30, CUHS20S40, CUHS20S30, CUHS15S40, CUHS15S30
A new window will open