May 4, 2011
High Output White LEDs Achieve High Luminous Efficiency- in One of the Thinnest Packages Available
IRVINE, Calif., — Toshiba America Electronic Components, Inc., (TAEC)* has announced the addition of a new series of LEDs. Using a new package design, TAEC has developed small high luminous flux white LEDs with high luminous efficiency. With a broad lineup ranging from high-efficient, high-output models to high-color rendering models, these LEDs can be used as light sources for a variety of lighting applications, including replacement lamps, architectural lighting, retail display, commercial/industrial, outdoor and residential lighting.
Ideal as a replacement for traditional fluorescent bulbs in general lighting applications, Toshiba's new high-output white LEDs provide one of the industry's highest level of efficiency at 120 lm/W, are housed in a very thin package (0.65 mm thick, making them suitable for small equipment) and have a long lifespan due to low thermal resistance. Additionally, a unique packaging structure and wide directional characteristics make these LEDs appropriate for lighting large areas.
** Based on Toshiba analysis (April 2011)
Type | Part number | Color temperature (K) | Luminous flux(lm) | Cx/Cy; | Luminous efficiency (lm/W); | Ra | Forward voltage (V) |
High efficiency type | TL19W01-D | 6500 | 110 | 0.313/0.329 | 110 | 65 | 3.3 |
TL19W01-N | 5000 | 120 | 0.345/0.355 | 120 | 65 | ||
TL19W01-W | 4000 | 110 | 0.382/0.38 | 110 | 65 | ||
TL19W01-WW | 3500 | 100 | 0.407/0.392 | 100 | 65 | ||
TL19W01-L | 3000 | 100 | 0.434/0.403 | 100 | 70 | ||
Medium color rendering type (Ra85) | TL19W01-NH1 | 5000 | 95 | 0.345/0.355 | 95 | 85 | |
TL19W01-WH1 | 4000 | 90 | 0.382/0.38 | 90 | 85 | ||
TL19W01-WWH1 | 3500 | 85 | 0.407/0.392 | 85 | 85 | ||
TL19W01-LH1 | 3000 | 85 | 0.434/0.403 | 85 | 85 | ||
High color rendering type | TL19W01-NH2 | 5000 | 90 | 0.345/0.355 | 90 | 92 | |
TL19W01-LH2 | 3000 | 80 | 0.434/0.403 | 90 | 92 |
The Toshiba White High Flux LEDs are available now. Budgetary pricing begins at $3.92, with volume discounts available.
Since 1986, Toshiba Corp. has ranked as the top discrete supplier on a worldwide basis, based on annual revenue from international shipments of total discrete products. According to the most recent annual report from market research firm Gartner Dataquest (San Jose, CA), Toshiba remained the top discrete semiconductor supplier. (Source: "2009 Worldwide Semiconductor Market Share Report," Gartner, released April 2010). More specifically, Toshiba is a leading supplier in a number of discrete product categories, including power transistors, rectifiers and thyristors, LMOS logic, CMOS logic, photocouplers, Toslinks TM , LEDs, small signal diodes and transistors. The company's discrete devices are designed to meet the growing demand for high-performance and lower voltages in today's wireless telecommunications and consumer electronics applications, while emphasizing its strength in the automotive and industrial markets.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, discrete devices, displays, advanced materials, medical tubes, custom SoCs/ASICs, digital multimedia and imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2009 WW Semiconductor Revenue, April 2010). Toshiba was founded in 1875, and today operates a global network of more than 740 companies, with 204,000 employees worldwide and annual sales surpassing $68 billion.
For additional company and product information, please visit http://www.toshiba.com/taec/ .
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba's "Handling Guide for Semiconductor Devices," or "Toshiba Semiconductor Reliability Handbook." This information is available at www.chips.toshiba.com, or from your TAEC representative.
Editor's Note: Product photos can be downloaded at
http://www.toshiba.com/taec/news/media_resources/news_mr_gallery.jsp
APIC 11 609