July 19, 2011
New Series Offers Industry's Lowest On-Resistance
IRVINE, Calif., — Toshiba America Electronic Components, Inc., (TAEC)* has announced the addition of the SSM6P47NU and SSM6P49NU to its lineup of small signal MOSFETS. Ideal for charging circuits for mobile devices, these dual Pch MOSFETS feature the lowest on-resistance in the industry when compared to equivalent packages.
From mobile phones and game consoles to digital cameras, power consumption and physical size are key considerations in the design of mobile devices. Toshiba's SSM6P47NU and SSM6P49NU address these issues by combining two independent transistors into one package.
A 1.8V drive, combined with a 4A drain current and extremely low on-resistance allow the SSM6P47NU and SSM6P49NU to run at a high rate of efficiency, which enables batteries to be fully charged in less time. Available in a UDFN6 package (2.0 x 2.0mm), these dual MOSFETs are a suitable size for charging circuits and are capable of acting as a switch to control which loads are connected or disconnected from the circuit.
SSM6P47NU | SSM6P49NU |
VDSS = -20V |
VDSS = -20V VGSS = ±12V ID = 4A RDS(max)@(VGS=-1.8V) = 157mΩ RDS(max)@(VGS=-2.5V) = 76mΩ RDS(max)@(VGS=-4.5V) = 56mΩ CISS(typ) = 480 pF |
The Toshiba SSM6P47NU and SSM6P49NU dual Pch MOSFETs are available now.
Toshiba is a leading supplier in a number of discrete product categories, including power transistors, rectifiers and thyristors, LMOS logic, CMOS logic, photocouplers, Toslinks™, LEDs, small signal diodes and transistors. The company's discrete devices are designed to meet the growing demand for high-performance and lower voltages in today's wireless telecommunications and consumer electronics applications, while emphasizing its strength in the automotive and industrial markets.
Through proven commitment, lasting relationships and advanced, reliable electronic components, Toshiba enables its customers to create market-leading designs. Toshiba is the heartbeat within product breakthroughs from OEMs, ODMs, CMs, distributors and fabless chip companies worldwide. A committed electronic components leader, Toshiba designs and manufactures high-quality flash memory-based storage solutions, discrete devices, displays, advanced materials, medical tubes, custom SoCs/ASICs, digital multimedia and imaging products, microcontrollers and wireless components that make possible today's leading cell phones, MP3 players, cameras, medical devices, automotive electronics and more.
Toshiba America Electronic Components, Inc. is an independent operating company owned by Toshiba America, Inc., a subsidiary of Toshiba Corporation, Japan's largest semiconductor manufacturer and the world's third largest semiconductor manufacturer (Gartner, 2010 WW Semiconductor Revenue, April 2011). Toshiba was founded in 1875, and today operates a global network of more than 490 companies, with 203,000 employees worldwide and annual sales of $77 billion. Visit Toshiba's web site at www.toshiba.co.jp/index.htm.
Information in this press release, including product pricing and specifications, content of services and contact information, is current and believed to be accurate on the date of the announcement, but is subject to change without prior notice. Technical and application information contained here is subject to the most recent applicable Toshiba product specifications. In developing designs, please ensure that Toshiba products are used within specified operating ranges as set forth in the most recent Toshiba product specifications and the information set forth in Toshiba’s “Handling Guide for Semiconductor Devices,” or "Toshiba Semiconductor Reliability Handbook."” This information is available at www.chips.toshiba.com, or from your TAEC representative.
LGSS 11 615